EAGLE User Chat (English) Pad Dilema
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 534 views
  • Users 0 members are here
Related

Pad Dilema

autodeskguest
autodeskguest over 16 years ago

Greetings,

 

I need advice for the following, I attached a 5 KB GIF drawing:

 

I want to place four pads on a board and connect one wire to each pad.

 

I want the four pads to be tied together on top and bottom layers with

either polygons or rectangles or something else.

 

I want the area on the finished board to appear as one big pad with four

through-holes in it. Bare copper with no mask over the area.

 

Each hole will have a wire attached and soldered in the final assembly and

all wires carry the same signal..

 

Should I use polygons or rectangles or something else to make this.

 

Thanks in advance for any help you can give me.

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Tilmann Reh" <user@domain.invalid> wrote in message

    news:gvimgl$qoo$1@cheetah.cadsoft.de...

    Biff schrieb:

     

    One thing I haven't figured out is how to connect a polygon to an "orphan

    pad" of a library device that has been placed on the board. But that's a

    whole nother can of worms.

     

    ...but answered quickly: it would represent a connection to a signal in

    the board, so this signal must also be present in the schematic.

     

    In EAGLE terminology, "orphan" pads must not be connected. Everything

    that is connected needs a pin in the schematic symbol. (However, pins of

    the symbol may be left unconnected.)

     

    Tilmann

     

    Thanks Much Tilmann. I really appreciate your input. Have an imaginary drink

    on me  ;^)

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

     

    "Tilmann Reh" <user@domain.invalid> wrote in message

    news:gvimgl$qoo$1@cheetah.cadsoft.de...

    Biff schrieb:

     

    One thing I haven't figured out is how to connect a polygon to an "orphan

    pad" of a library device that has been placed on the board. But that's a

    whole nother can of worms.

     

    ...but answered quickly: it would represent a connection to a signal in

    the board, so this signal must also be present in the schematic.

     

    In EAGLE terminology, "orphan" pads must not be connected. Everything

    that is connected needs a pin in the schematic symbol. (However, pins of

    the symbol may be left unconnected.)

     

    Tilmann

     

    Thanks Much Tilmann. I really appreciate your input. Have an imaginary drink

    on me  ;^)