Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Have choice of 16 layers on 2-layer board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 600 views
  • Users 0 members are here
Related

Have choice of 16 layers on 2-layer board

autodeskguest
autodeskguest over 17 years ago

I have a licensed version of Eagle 5.x.  A board is setup for 2 layers in the DRC using "(1*16)" where the graphics,

numbers, copper and isolation all show 2 layers.  The board is laid out with 2 layers.  Typing "cha lay" or the middle

mouse button shows the usual list plus unwanted layers 2-15.  To add insult to injury, a co-worker has an unlicensed

version and it lists only layers 1 and 16 on both his computer and if I copy his whole project over to mine.  Is there

any way to make the unwanted layers go away?  It would speed up hand routing sensitive nets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    I attached the script that I use to set up layers and views. It was renamed

    to a .txt filext for easy viewing with a text viewer. You should be able to

    pick it apart and delete what you don't want to use. When done, rename to a

    .scr and put in your scripts directory. Always a good idea to never send

    anything as a .scr which can as easily be a virus.

        Oppie

     

    "Alan" <astummer@physics.utoronto.ca> wrote in message

    news:h1t4mm$g3d$1@cheetah.cadsoft.de...

    I have a licensed version of Eagle 5.x.  A board is setup for 2 layers in

    the DRC using "(1*16)" where the graphics, numbers, copper and isolation

    all show 2 layers.  The board is laid out with 2 layers.  Typing "cha lay"

    or the middle mouse button shows the usual list plus unwanted layers 2-15.

    To add insult to injury, a co-worker has an unlicensed version and it

    lists only layers 1 and 16 on both his computer and if I copy his whole

    project over to mine.  Is there any way to make the unwanted layers go

    away?  It would speed up hand routing sensitive nets.

     

    Attachments:
    mylayers[bob].txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Thanks, that fix is simple and works.  The issue was only annoying, not functional.

     

    James Morrison wrote:

    Alan Stummer wrote on Wed, 24 June 2009 08:03

    I have a licensed version of Eagle 5.x.  A board is setup for 2 layers

    in the DRC using "(1*16)" where the graphics,

    numbers, copper and isolation all show 2 layers.  The board is laid out

    with 2 layers.  Typing "cha lay" or the middle

    mouse button shows the usual list plus unwanted layers 2-15.  To add

    insult to injury, a co-worker has an unlicensed

    version and it lists only layers 1 and 16 on both his computer and if I

    copy his whole project over to mine.  Is there

    any way to make the unwanted layers go away?  It would speed up hand

    routing sensitive nets.

     

     

    Hi Alan,

     

    Yes, there is a way to do this.  I have found that if I go in and edit the

    DRC layer setting and then apply it then all those other layers will go

    away.  What I do is change the "1*16" to "1+16" or vice versa, can't

    remember off the top of my head.  Then the layers go away.  Since I don't

    really care (in EAGLE) that the board is specified with core or prepreg it

    works fine.

     

    I don't work with 2 layers all that often so I don't hit this often.  But

    I consider it a bug that should be fixed.  If the DRC says 2 layers then it

    shouldn't show you 16 options for layers.

     

    Cheers,

     

    James.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Alan schrieb:

     

    I have a licensed version of Eagle 5.x.  A board is setup for 2

    layers in the DRC using "(1*16)" where the graphics, numbers, copper

    and isolation all show 2 layers.  The board is laid out with 2

    layers.  Typing "cha lay" or the middle mouse button shows the usual

    list plus unwanted layers 2-15.  To add insult to injury, a co-worker

    has an unlicensed version and it lists only layers 1 and 16 on both

    his computer and if I copy his whole project over to mine.  Is there

    any way to make the unwanted layers go away?  It would speed up hand

    routing sensitive nets.

     

    Use the command "SET USED_LAYERS" to mask away all unwanted layers.

    I have set up a script file to do this for two- or four-layer boards so

    I don't need to type all wanted layers each time I start a new design.

     

    Tilmann

     

    P.S. Please correct your line length (and turn off format=flawed).

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Alan Stummer wrote on Wed, 24 June 2009 08:03

    I have a licensed version of Eagle 5.x.  A board is setup for 2 layers

    in the DRC using "(1*16)" where the graphics,

    numbers, copper and isolation all show 2 layers.  The board is laid out

    with 2 layers.  Typing "cha lay" or the middle

    mouse button shows the usual list plus unwanted layers 2-15.  To add

    insult to injury, a co-worker has an unlicensed

    version and it lists only layers 1 and 16 on both his computer and if I

    copy his whole project over to mine.  Is there

    any way to make the unwanted layers go away?  It would speed up hand

    routing sensitive nets.

     

     

    Hi Alan,

     

    Yes, there is a way to do this.  I have found that if I go in and edit the

    DRC layer setting and then apply it then all those other layers will go

    away.  What I do is change the "1*16" to "1+16" or vice versa, can't

    remember off the top of my head.  Then the layers go away.  Since I don't

    really care (in EAGLE) that the board is specified with core or prepreg it

    works fine.

     

    I don't work with 2 layers all that often so I don't hit this often.  But

    I consider it a bug that should be fixed.  If the DRC says 2 layers then it

    shouldn't show you 16 options for layers.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    email:  sales2009@eaglecentral.ca

    fax:    888.701.8097

    web:    http://www.eaglecentral.ca

     

    Online EAGLE Dealer for US and Canada

    EAGLE Design Experts

    EAGLE Enterprise Toolkit

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca