Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Tip: fast search in libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 560 views
  • Users 0 members are here
  • search
  • libraries
  • grep
Related

Tip: fast search in libraries

Joop14
Joop14 over 12 years ago

When I'm looking for a footprint (or something else) in the libraries, I found that it is much faster to open a console (terminal) in the library directory and enter the following command:

 

grep -i so8 *.lbr

 

This will show which libraries contain the string so8 or SO8.

 

Ofcourse,  this only works from Eagle version 6.xx and up which stores the libraries in XML.

 

In the unfortunate case that you have been forced to use the windows OS, grep is not installed by default.

In that case you can download it here: Grep for Windows

 

Have a nice day,

 

Joop

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    On 8/9/2014 5:24 AM, Joop14 wrote:

    When I'm looking for a footprint (or something else) in the libraries, I

    found that it is much faster to open a console (terminal) in the library

    directory and enter the following command:

     

    grep -i so8 *.lbr

     

    This will show which libraries contain the string so8 or SO8.

     

    Ofcourse,  this only works from Eagle version 6.xx and up which stores

    the libraries in XML.

     

    In the unfortunate case that you have been forced to use the windows OS,

    grep is not installed by default.

    In that case you can download it here: Grep for Windows

    (http://gnuwin32.sourceforge.net/packages/grep.htm)

     

     

    Hi Guys,

     

    You can also search for packages in the board editor's ADD command,

    avoiding the need for a third party tool. Most of the common packages

    are in the ref-packages.lbr so it's always a good place to start.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 12 years ago in reply to autodeskguest

    You can also search for packages in the board editor's ADD command,

    avoiding the need for a third party tool.

     

    1. Many times, when I'm creating new devices, I don't have a schematic or board opened so I can not use the ADD command.

     

    2. On Linux, grep is installed by default.

     

    3. In my case, when using the ADD command for searching, it does not find the libraries provided by Cadsoft Eagle because I removed the eagle/lbr directory from the path's in the settings. Instead I created and added a directory eagle/lbr2 where I put the libraries I use. This way, Eagle loads a project much faster.

    (When alI libraries are included in the project file (*.epf), Eagle becomes slow when opening a project.

    When you want to try this, make sure you remove the library path's from the project file (you have to edit it manually).

     

    Best Regards,

     

    Joop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Joop14
    Joop14 over 12 years ago in reply to autodeskguest

    You can also search for packages in the board editor's ADD command,

    avoiding the need for a third party tool.

     

    1. Many times, when I'm creating new devices, I don't have a schematic or board opened so I can not use the ADD command.

     

    2. On Linux, grep is installed by default.

     

    3. In my case, when using the ADD command for searching, it does not find the libraries provided by Cadsoft Eagle because I removed the eagle/lbr directory from the path's in the settings. Instead I created and added a directory eagle/lbr2 where I put the libraries I use. This way, Eagle loads a project much faster.

    (When alI libraries are included in the project file (*.epf), Eagle becomes slow when opening a project.

    When you want to try this, make sure you remove the library path's from the project file (you have to edit it manually).

     

    Best Regards,

     

    Joop