EAGLE User Chat (English) Problem with con-wago.lbr
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 264 views
  • Users 0 members are here
Related

Problem with con-wago.lbr

autodeskguest
autodeskguest over 16 years ago

Using the CON-WAGO.LBR part 233-502 in the schematics the numbers 1 and 2

are obscured by the symbol.

Opening the library and the symbol in that shows the same but moving the

numbers has no result.

 

How can i move the numbers so that they can be read.

 

Harry

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 16 years ago

    Harry H. Arends schrieb:

    Using the CON-WAGO.LBR part 233-502 in the schematics the numbers 1 and

    2 are obscured by the symbol.

    Opening the library and the symbol in that shows the same but moving the

    numbers has no result.

     

    How can i move the numbers so that they can be read.

     

    Harry

     

     

    There are lined up two pins in order to connect both pads in

    the package. The first pin shows its name and this is too close

    at the end of the second pin.

    You could either switch off diplaying the pin name (change visible off)

    and write/place the text with the TEXT command or re-arrange the pins

    so that the text is better readable.

     

    I will forward this to our librarian....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm