Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) component is not aligned to grid
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 249 views
  • Users 0 members are here
Related

component is not aligned to grid

autodeskguest
autodeskguest over 16 years ago

Hi,

 

I created a library for a TQFP-128 fine pitch part with 0,4mm pitch size.

For this reason in the library package I used a 0,4mm grid as well.

 

In my project's layout, where I want to use that part, I also have a

0,4mm grid size so that it works together with the package I created.

 

However, if I place the part on the PCB layout multiple times, not all

parts are aligned to the 0,4mm layout grid.

Since both the layout grid size as well as the package grid size in the

library are 0,4mm, this should not happen, right ?

 

Since it is a little hard to explain I uploaded a picture here:

http://img404.imageshack.us/img404/1152/misaligned04mmpitchcomp.png

 

Unfortunately in the picture one can't see the 0,4mm grid.

However, while the upper left chip package is perfectly aligned to the

grid, the other three packages are not.

I tried to place them in a way that all chip pins are perfectly aligned

to each other, but as you can see this was not possible.

 

 

A dirty solution would be to switch to a smaller grid size in the layout

(e.g. 0,1mm).

 

However, I would prefer to use the bigger 0,4mm grid so that layout

design is easier to work with.

 

Is this a bug in eagle ?

I'm using Eagle 5.6.0 Light.

 

sincerely,

stefan

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Hi,

     

    the problem is solved.

    The solution is to press the Ctrl key before moving the object which

    causes the object to be snapped into the current grid.

     

    For reference see "Selecting objects at their origin" in the help page

    for move.

     

    cheers,

    stefan