EAGLE User Chat (English) radial copy
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 407 views
  • Users 0 members are here
Related

radial copy

Former Member
Former Member over 16 years ago

Hello,

I'm building a package in 5.6 and I want to place pads in a circle. Is there

a way to have each pad an equal distance from the previous one and declare

how many pads are in the 360 degree circle. Let's say I wanted a circle with

15 pads in it.

Thanks for the help,

Rob

 

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 16 years ago

    Rob schrieb:

    Hello,

    I'm building a package in 5.6 and I want to place pads in a circle. Is there

    a way to have each pad an equal distance from the previous one and declare

    how many pads are in the 360 degree circle. Let's say I wanted a circle with

    15 pads in it.

    Thanks for the help,

    Rob

     

     

     

     

    You can place the pads with using polar coordiantes.

    Set a relative origin with the MARK command and type in the coordinates

    in the command line, for example:

     

    pad (P10 0)

    pad (P10 15)

    pad (P10 30)

    pad (P10 45)

    ....

    ....

    ....

    This places pads with a radius of 10 in 15 degree steps around the

    relative origin.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 16 years ago

    On 10/16/2009 04:41 AM, Richard Hammerl wrote:

    Rob schrieb:

    Hello,

    I'm building a package in 5.6 and I want to place pads in a circle.

     

    You can place the pads with using polar coordiantes.

    Set a relative origin with the MARK command and type in the coordinates

    in the command line, for example:

     

    pad (P10 0)

    pad (P10 15)

    pad (P10 30)

    pad (P10 45)

    ....

    ....

     

    This is what I had to do to place LEDs on a light ring for a microscope.

    I also added a rotation for each LED to keep the leads tangent to the

    circle on which the part was placed:

     

    rotate =R0 LED1

    rotate =R15 LED2

    rotate =R30 LED3

    ...

     

    Enjoy,

        - Chuck