Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Can't attach name or label to part pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 1814 views
  • Users 0 members are here
Related

Can't attach name or label to part pins

autodeskguest
autodeskguest over 11 years ago

I'm editing a previously downloaded part but for some reason I can't

select the NAME tool and click on a pin or attach a bus/net label.

I can attach a wire, then a label, but if I click on the next pin it

only attaches it to the previous pin!

I believe the original part (before my editing) worked the same way, so

maybe it has something to do with the actual part which is a PCB

card-edge (connecting fingers for a slot-card) as there aren't any

connection pins on the part in the PCB section.

As far as I can see the schematic pins and the PCB section are connected

though... what am I doing wrong?

I'm using Eagle 7.3.0. on a Mac

 

L.

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 06/06/2015 02:53 PM, Logyx wrote:

    On 04/06/2015 01:45, Warren Brayshaw wrote:

     

    I suggest you check you have used a grid size of 0.1 inch in both the

    library and the schematic. That is the accepted default and the only way

    you can connect to pins.

     

    What should I do with metric parts?

    I'm currently designing a card-edge connector part (something like this:

    http://www.eurocircuits.com/blog/40-connectors) which of course won't

    "snap" into an imperial grid.

    What I've done when designing it is change the grid to mm, but it needs

    to fit in together with the other components when designing a PCB.

     

    To clarify.

    Lib symbol and schematic are 0.1" grid. Layout and pads are set to the

    data sheet.

    When routing having your grid in layout just small enough so the metric

    and non metric pads are almost on your grid.

    Paul R

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 04/06/2015 01:45, Warren Brayshaw wrote:

     

    I suggest you check you have used a grid size of 0.1 inch in both the

    library and the schematic. That is the accepted default and the only way

    you can connect to pins.

     

    What should I do with metric parts?

    I'm currently designing a card-edge connector part (something like this:

    http://www.eurocircuits.com/blog/40-connectors) which of course won't

    "snap" into an imperial grid.

    What I've done when designing it is change the grid to mm, but it needs

    to fit in together with the other components when designing a PCB.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 04/06/15 06:34, Logyx wrote:

     

    So, I've figured out that I can't simply choose the LABEL tool and just

    click on the pins but have to attach a WIRE or NET first, using those

    tools.

     

    Correct. You can assign a name to a whole part, but not to a pin.

    However, pins exist for connecting to nets, which you can then name.

     

     

    What's the difference between those two tools? They seem to do the same

    thing.

     

    The WIRE tool is not intended for making electrical connections (yes,

    it's a confusing name). It would be better called "LINE" because it

    draws lines. It can be used on any layer for documentation purposes.

     

    The NET tool is the one you should use to form electrical connections.

    It has additional functionality, such as automatically stopping when you

    click on a pin, and automatically adding junctions if you end on another

    net.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 04/06/2015 01:45, Warren Brayshaw wrote:

    Your description is confusing as you talk of editing a part, which can only

    be done in a library, and in the same sentence you do things that can only

    be done in a Schematic.

     

    Sorry about the confusion.

    I meant I couldn't connect a net label to the part while in the schematic.

     

     

    I suggest you check you have used a grid size of 0.1 inch in both the

    library and the schematic. That is the accepted default and the only way

    you can connect to pins. Use the NET tool and not the WIRE tool when

    connecting to pins

     

    The grid size of the part and in the schematic is set to the default value.

     

    Aha! I believe my problem arose because I just didn't understand how to

    add labels the right way. I'm trying to join two 40 pin connectors

    together without making a mess, which is why that would be useful.

     

    So, I've figured out that I can't simply choose the LABEL tool and just

    click on the pins but have to attach a WIRE or NET first, using those

    tools. Also, I had forgotten to deselect the (not hightlight in green)

    the pin I was previously working on before adding a new label.

     

    What's the difference between those two tools? They seem to do the same

    thing.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Your description is confusing as you talk of editing a part, which can only

    be done in a library, and in the same sentence you do things that can only

    be done in a Schematic.

     

    I suggest you check you have used a grid size of 0.1 inch in both the

    library and the schematic. That is the accepted default and the only way

    you can connect to pins. Use the NET tool and not the WIRE tool when

    connecting to pins

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.