Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Board inconsistency -how to update?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 187 subscribers
  • Views 1747 views
  • Users 0 members are here
Related

Board inconsistency -how to update?

autodeskguest
autodeskguest over 11 years ago

I'm experiencing inconsistencies with a board.

In the past I've simply deleted the board file then created a new one

from the schematic, but in this case I've spent considerable time with

the layout.

 

Is there a way to "synchronize" the board file with the current schematic?

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 08/06/15 07:48, Logyx wrote:

    I'm experiencing inconsistencies with a board.

    In the past I've simply deleted the board file then created a new one

    from the schematic, but in this case I've spent considerable time with

    the layout.

     

    Is there a way to "synchronize" the board file with the current schematic?

     

    They are automatically kept in synch as long as you have both open

    whenever you make a change. Eagle defaults to always opening both (or at

    least offers to, you can sometimes say no).

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 08/06/2015 09:30, Rob Pearce wrote:

    On 08/06/15 07:48, Logyx wrote:

     

    Is there a way to "synchronize" the board file with the current schematic?

     

    They are automatically kept in synch as long as you have both open

    whenever you make a change. Eagle defaults to always opening both (or at

    least offers to, you can sometimes say no).

     

    Yes, I know, but they have come out of sync. Probably because I disabled

    the board file (renamed its extension to ._RD) when I should have made a

    backup copy instead, replaced parts etc.

     

    Basically, I don't want to lose the board layout I have in that file,

    but want to update it to be consistent with the schematic. Is there a

    way to force a synchronization between the two?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 08/06/2015 09:30, Rob Pearce wrote:

    On 08/06/15 07:48, Logyx wrote:

     

    Is there a way to "synchronize" the board file with the current schematic?

     

    They are automatically kept in synch as long as you have both open

    whenever you make a change. Eagle defaults to always opening both (or at

    least offers to, you can sometimes say no).

     

    Yes, I know, but they have come out of sync. Probably because I disabled

    the board file (renamed its extension to ._RD) when I should have made a

    backup copy instead, replaced parts etc.

     

    Basically, I don't want to lose the board layout I have in that file,

    but want to update it to be consistent with the schematic. Is there a

    way to force a synchronization between the two?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Am 09.06.2015 um 14:32 schrieb Logyx:

    On 08/06/2015 13:46, Werner wrote:

    Am 08.06.2015 um 10:27 schrieb Logyx:

    Basically, I don't want to lose the board layout I have in that file,

    but want to update it to be consistent with the schematic. Is there a

    way to force a synchronization between the two?

     

     

    HI,

    if you run "ERC" so you get a list of the diffs between board

    an schematic.

    Then you can do the changes by hand. If you have done all

    errors the "ERC" make flags the board and schematic as sync.

     

    Yes, I do get several errors when pressing "ERC" in the schematic, such

    as consistency errors: "Part xx not found in board" and warnings: "Only

    one pin on net xx".

    So I go to the board, add the first missing component and naming it the

    same as in the schematic. I was hoping to see the wires magically appear

    but not so. And in the schematic I still get the same errors.

    How should I proceed?

     

     

    L.

    Hi,

    the Warning with one pin is in the schematic.

    Look at the Net "Show netname".

    If you see that the net is highighted and the pins not, move the symbol

    a little bit away and back to the Net. It will be connect to the symbol.

    (If not check Grid etc.)

    The wires will be "magically appear" in the board if you use "export

    Netscript"(Help Netscript would be your friend). Then run the exported

    script in the  board....

     

    HTH (HopeThatHelps)

    Werner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 08/06/2015 13:46, Werner wrote:

    Am 08.06.2015 um 10:27 schrieb Logyx:

     

    Basically, I don't want to lose the board layout I have in that file,

    but want to update it to be consistent with the schematic. Is there a

    way to force a synchronization between the two?

     

     

    HI,

    if you run "ERC" so you get a list of the diffs between board

    an schematic.

    Then you can do the changes by hand. If you have done all

    errors the "ERC" make flags the board and schematic as sync.

     

    Yes, I do get several errors when pressing "ERC" in the schematic, such

    as consistency errors: "Part xx not found in board" and warnings: "Only

    one pin on net xx".

    So I go to the board, add the first missing component and naming it the

    same as in the schematic. I was hoping to see the wires magically appear

    but not so. And in the schematic I still get the same errors.

    How should I proceed?

     

     

    L.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Am 08.06.2015 um 10:27 schrieb Logyx:

    On 08/06/2015 09:30, Rob Pearce wrote:

    On 08/06/15 07:48, Logyx wrote:

    Is there a way to "synchronize" the board file with the current

    schematic?

     

    They are automatically kept in synch as long as you have both open

    whenever you make a change. Eagle defaults to always opening both (or at

    least offers to, you can sometimes say no).

     

    Yes, I know, but they have come out of sync. Probably because I disabled

    the board file (renamed its extension to ._RD) when I should have made a

    backup copy instead, replaced parts etc.

     

    Basically, I don't want to lose the board layout I have in that file,

    but want to update it to be consistent with the schematic. Is there a

    way to force a synchronization between the two?

     

     

    HI,

    if you run "ERC" so you get a list of the diffs between board

    an schematic.

    Then you can do the changes by hand. If you have done all

    errors the "ERC" make flags the board and schematic as sync.

     

    HTH

    Werner