Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Missing help or help files?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 499 views
  • Users 0 members are here
Related

Missing help or help files?

azark556
azark556 over 10 years ago

I'm not new to Eagle, but rather rusty.  Just got version 7 and computer went belly up, so had to reinstall 7.6 on my Linux Mint 18 machine.  Install seemed to go well and everything seems to be working except for getting help from the menu.  Nothing appears.  Missing files?  Wrong place? Any suggestions?

Don

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Tutorial

     

    Is part of the EAGLE installation and can be found in the doc folder as a pdf file. Perfect for a newbie to get familiar with EAGLE.

    Manual

     

    Is also part of the EAGLE installation and available as pdf file in the doc folder.

    Help Function

     

    Can be used any time in EAGLE. Start it either through the Help menu, or by using the F1 key, or typing HELP in the command line of an Editor window. HELP ROUTE for example, shows the help page for the ROUTE command.

    From: https://cadsoft.io/support/faq/#0

    Check folders for these to see if install worked.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Tutorial

     

    Is part of the EAGLE installation and can be found in the doc folder as a pdf file. Perfect for a newbie to get familiar with EAGLE.

    Manual

     

    Is also part of the EAGLE installation and available as pdf file in the doc folder.

    Help Function

     

    Can be used any time in EAGLE. Start it either through the Help menu, or by using the F1 key, or typing HELP in the command line of an Editor window. HELP ROUTE for example, shows the help page for the ROUTE command.

    From: https://cadsoft.io/support/faq/#0

    Check folders for these to see if install worked.

    Clem