Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) PCB Power (On/Off) Switch and Fuse Recommendation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 3946 views
  • Users 0 members are here
Related

PCB Power (On/Off) Switch and Fuse Recommendation

dhofer
dhofer over 8 years ago

Hello All,

 

This is my first post here and admittedly, I am new to the Eagle CAD world.  I recently hired a freelancer to convert a breadboard design to a PCB using Eagle and he specified a RDT1034 switch (3 pin) and I can not find a reasonable replacement.  Can you point me to a good replacement/alternative?  

 

He also placed a fuse after the switch and before the VI of the 3.3v voltage regulator.  I'm also looking for a reference to a suitable fuse part number.

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 8 years ago

    Dave,

     

    First off, welcome to the community. There are several active people here willing to help and be helped.

     

    Switches are extremely plentiful in their size, shape and function.  I could not find any info on RDT1034 part, so I am not sure that I can help you with this part.  If you have more information, like a specification sheet, or even a snapshot of the switch in the schematic and layout, it might be able to help in understanding the form/fit/function that is needed.

     

    The fuse is also problematic, in that fuses come in many varieties and have several parameters (trip/blow current, slow/fast blow, physical dimensions).  Again, a better understanding of the design would be helpful to select a proper component (same as above, more information would help).

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dhofer
    0 dhofer over 8 years ago in reply to genebren

    Thanks Gene.  I appreciate the feedback and help!  My freelancer was from Russia (I think, his profile said US...) and used older libraries.  I am trying to use components that are available in an Eagle Library and that I have an exact part number to place on the board and order.  I'm getting wrapped around the axle on that point.

     

    The RDT1034 in the board looks like this (no other property values are available):

     

    image

     

    This is how he laid out the power-in for the schematic.   Honestly, since I'm using a barrel jack, I really don't need the switch and my breadboard currently has no fuse.  So, from a prototyping perspective, I could probably just eliminate them for now.  But, it's got to be better to have them even if it's a prototype board.

    image

    I suspect that there are a thousand suitable replacements for the RDT1034.   For example, this one:

     

    image

     

    I think this is what he specified for the fuse holder.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to dhofer

    Dave,

     

    It gets a little weird when you work with some people in remote locations and they are using older versions of the software.

     

    Depending on how you deploy your design, yeah the switch might not be necessary.  If you are going to use a switch now, the one you linked to could be used if you are wiring it in remotely, as the footprint on the layout does not match with this switch.  If you are intending to mount the switch on the PCB, you will need another switch.

     

    On the topic of fuses, it is still difficult to determine the value of the fuse that would be needed, without understanding the expected current draw.  The line of fuses for use with this holder range from 40mA all the way up to 10A.  You need to pick one that would cover your normal range of operation, which some headroom for inrush or other surges (within normal operation). I am a little ashamed to say this, but on low-voltage boards, like this, I do not usually install a fuse.  If there were some regulatory requirements that needed to be met, I would, but for the most part that has not been the case.  The protective device in most cases is the attached power supply.  Most are capable of shutting down on an over-current situation.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to genebren

    On Thu, 18 Jan 2018 21:40:20 GMT, Gene Breniman

     

    If protection is needed, ditch the fuse and use a polyfuse instead.

    This is a specially designed thermistor that "opens" at a designated

    amperage but resets when it cools off.

     

    John

     

    wrote:

     

    On the topic of fuses, it is still difficult to determine the value of the fuse that would be needed, without understanding the expected current draw.  The line of fuses for use with this holder range from 40mA all the way up to 10A.  You need to pick one that would cover your normal range of operation, which some headroom for inrush or other surges (within normal operation). I am a little ashamed to say this, but on low-voltage boards, like this, I do not usually install a fuse.  If there were some regulatory requirements that needed to be met, I would, but for the most part that has not been the case.  The protective device in most cases is the attached power supply.  Most are capable of shutting down on an over-current situation.

     

    Good luck,

    Gene

    John DeArmond

    http://www.neon-john.com

    http://www.tnduction.com

    Tellico Plains, Occupied TN

    See website for email address

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 8 years ago in reply to genebren

    On Thu, 18 Jan 2018 21:40:20 GMT, Gene Breniman

     

    If protection is needed, ditch the fuse and use a polyfuse instead.

    This is a specially designed thermistor that "opens" at a designated

    amperage but resets when it cools off.

     

    John

     

    wrote:

     

    On the topic of fuses, it is still difficult to determine the value of the fuse that would be needed, without understanding the expected current draw.  The line of fuses for use with this holder range from 40mA all the way up to 10A.  You need to pick one that would cover your normal range of operation, which some headroom for inrush or other surges (within normal operation). I am a little ashamed to say this, but on low-voltage boards, like this, I do not usually install a fuse.  If there were some regulatory requirements that needed to be met, I would, but for the most part that has not been the case.  The protective device in most cases is the attached power supply.  Most are capable of shutting down on an over-current situation.

     

    Good luck,

    Gene

    John DeArmond

    http://www.neon-john.com

    http://www.tnduction.com

    Tellico Plains, Occupied TN

    See website for email address