Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) How to detect a 'usable' layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 3 answers
  • Subscribers 188 subscribers
  • Views 2492 views
  • Users 0 members are here
Related

How to detect a 'usable' layer?

fatbeard
fatbeard over 6 years ago

running 5.12.0

Inside an ULP I want to know what layers in a board are available.

When I loop through the layers in a board with an ULP (like: board(B) B.layers(L) {some code using L} ) I get all signal layers; the layer list in the board editor only shows the ones defined in the DRC.The ones not defined in the DRC are reported as hidden to the ULP.

When a script tries to access one of the layers not listed in the editor, an error pops up stating that that layer is not available (which is IMO correct) and continues to use the next available layer.

 

Is there a way for an ULP to detect if a hidden layer is just hidden or not available at all, to prevent this from happening in a generated script?

  • Sign in to reply
  • Cancel
Parents
  • WarrenBrayshaw
    0 WarrenBrayshaw over 6 years ago

    What are you trying to achieve with this ULP?. What's the problem it will solve for you? I suspect there may be a different approach possible.

     

    You cannot determine the layers available by cycling through the Board object. As you have noticed, they are all listed there. You can only report if a layer is unused (dirty) and if it is being displayed (visible) or not.

    Which layers you can you can write to depends on the Eagle Edition you have.

     

    Which layers are shown with a ulp by cycling through the Board object. depends on the Edition and the source of the board file. In the Light version , a board started there only returns layers 1 and 16. But I can load a 2 layer board made in a 16 layer edition and it returns 16 layers.

     

    Note that you can open a 16 layer board in the Light (2 layers) version. You see the full design (16 layers in the layer drop down) but in the Light version you can only edit layers 1 and 16.of that design.

     

    Even reading the layer setup in the DRC does not help because that can be for a 2 layer board in a 16 layer capable edition. and visa versa.

     

    So for a script that must run on different editions, it must determine which layers are valid for that edition.

     

    Are you are saying that a 'usable layer' must be a layer quoted in the DRC layer setup ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • WarrenBrayshaw
    0 WarrenBrayshaw over 6 years ago

    What are you trying to achieve with this ULP?. What's the problem it will solve for you? I suspect there may be a different approach possible.

     

    You cannot determine the layers available by cycling through the Board object. As you have noticed, they are all listed there. You can only report if a layer is unused (dirty) and if it is being displayed (visible) or not.

    Which layers you can you can write to depends on the Eagle Edition you have.

     

    Which layers are shown with a ulp by cycling through the Board object. depends on the Edition and the source of the board file. In the Light version , a board started there only returns layers 1 and 16. But I can load a 2 layer board made in a 16 layer edition and it returns 16 layers.

     

    Note that you can open a 16 layer board in the Light (2 layers) version. You see the full design (16 layers in the layer drop down) but in the Light version you can only edit layers 1 and 16.of that design.

     

    Even reading the layer setup in the DRC does not help because that can be for a 2 layer board in a 16 layer capable edition. and visa versa.

     

    So for a script that must run on different editions, it must determine which layers are valid for that edition.

     

    Are you are saying that a 'usable layer' must be a layer quoted in the DRC layer setup ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fatbeard
    0 fatbeard over 6 years ago in reply to WarrenBrayshaw

    Well, I bit the bullet so to speak and hacked a bit into the binary (after all, the board file is the only thing I'm certain of when the ULP is running)...

     

    In short, it turns out that the binary is structured into records of 24 bytes; the first byte being the record type: type 0x13 is a layer definition where byte 3 is the layer number.

    Byte 2 contains flags: bit 0 tells if the layer is valid for this editor and bit 1 tells if the layer is editable (active).

    The layer name is only inside the record if it is 9 characters or shorter (and not easy to extract otherwise), but a layers() loop will get the name easy enough.

    This functions well, although this may not work as expected if the Eagle license does not allow all layers listed in the board's DRC (I have currently no way of testing this).

     

    From what I see in later versions that use the easier to parse XML format, the critical layer parameter there is "active" (albeit that I do not have much to compare here).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fatbeard
    0 fatbeard over 6 years ago in reply to WarrenBrayshaw

    This ULP I'm working on is to import a DXF file into an Eagle object; be it a board, schematic, symbol or package.

    It offers a choice of what and how to import, a choice for the layer to put it on, various scaling and offset options and in a library environment a choice for the package or symbol to put it in ('new' being an option).

    This all functions well, except for the layer list in the board environment: you can select a layer that is not in the DRC list (and thus not editable).In that case the generated script fails and I want to prevent that.

     

    Generating a correct layer list for the package, symbol and schematic is easy enough: all layers reported by the layer() loop are fair game (barring the obvious nogo ones).

    In the board the DRC setup complicates matters, since it effectively 'cancels out' some of the reported layers.

    Parsing the board file in the ULP is an option: I know what to look for; I just hope that it can be avoided.

     

     

    I was (and still am) looking for an easier way to produce the correct layer list to choose from in a board environment...