Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Exporting Eagle PCB's and Schematics from and into other formats.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 3155 views
  • Users 0 members are here
Related

Exporting Eagle PCB's and Schematics from and into other formats.

e14 Contributor
e14 Contributor over 15 years ago

Does anyone have any suggestions or information about converting PCB or Schematic files from Eagle into other program formats?  Or reading any from any other software into Eagle?

 

 

Any information related to  Allegro, or Cadstar or Orcad or Pads or P-Cad, or just about any other format would be appreciated.

 

Thanks

  • Sign in to reply
  • Cancel
  • leon_heller
    0 leon_heller over 15 years ago

    The Pulsonix software I use is supplied with ULPs to convert Eagle schematics, PCBs, and libraries so that they can be imported. The process works very well with the current version of Eagle, even though the ULPs haven't been updated for a few years.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Joe Adler wrote on Tue, 08 February 2011 14:25

    Not at all.

    I like to use Cadsoft to make my boards and designs.

    After I am finished, it is useful to be able to send it them  a

    customer that prefers a different software package.

     

     

    Hi Joe,

     

    Anyone can use EAGLE as a design viewer, so if you have customers that

    simply need to look at the designs then they can use the freeware version

    of EAGLE.  If the read-only functionality is being used for profit

    (creating manuals, documenting for production, etc) then they should

    purchase the inexpensive

    http://www.eaglecentral.ca/purchase/eagle_light.php?product=1&d=1.

     

    Now if you really do want to translate the design into another format then

    that is another matter.  These designs are not simple documents and CAD

    formats differ quite dramatically and often aren't documented publicly (so

    you can't translate).  You should also know that nothing in the download

    directory at CadSoft is supported.  In fact, those ULP's can become stale

    and I've run into some that don't even work with EAGLE 5 now.  So you may

    find something to help or you may just be frustrated.

     

    If you want a professional translation then LogicSwap is a company that

    does professional CAD translation.  I've been working with them to develop

    their EAGLE output filter so that they can output EAGLE designs (libraries,

    schematic, and pcb's).  They also now have an EAGLE input filter I'm told.

     

    You can see more info at

    http://www.logicswap.com/datasheets/LS_Eagle_Services_Broch.pdf

     

    Hope that helps,

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Not at all.

    I like to use Cadsoft to make my boards and designs.

    After I am finished, it is useful to be able to send it them  a customer that prefers a different software package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to Richard_H

    "Richard Hammerl" <ric@cadsoft.de> wrote in message

    news:iiqqlt$har$2@cheetah.cadsoft.de...

    Am 07.02.2011 23:30, schrieb Morten Leikvoll:

    >> Joe Adler <jadler54@charter.net> wrote:

    >>> Does anyone have any suggestions or information about converting PCB or

    >>> Schematic files from Eagle into other program formats?  Or reading any

    >>> from any other software into Eagle?

    >>

    >>

    >> Isnt this a bit like asking a VW salesman where you can buy a Volvo?

    >> Yes, Im sure the support of the other apps will help you out.

     

    Perhaps he only wants to have a test drive and will come back

    afterwards, convinced that he will stay with what he has  image image  SCNR

     

    Hopefully image I've been down the Altium route myself, and Altium has some

    nice function that Eagle can't do (yet), but even if Altium has dropped a

    bit in price, the service fee for 1 year alone covers a separate full

    professional Eagle license image

    I have even seen competing sales people trying to make fun of Eagle!

    Having said that, being a programmer adds a LOT of value to Eagle. For

    simple boards, this is not an issue, but to do advanced modern lauout with

    it you need some programming skills imho.

    I am VERY exited to see what v6 will be able to do image

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 15 years ago in reply to e14 Contributor

    Am 07.02.2011 23:30, schrieb Morten Leikvoll:

    Joe Adler <jadler54@charter.net> wrote:

    >> Does anyone have any suggestions or information about converting PCB or

    >> Schematic files from Eagle into other program formats?  Or reading any

    >> from any other software into Eagle?

     

    Isnt this a bit like asking a VW salesman where you can buy a Volvo?

    Yes, Im sure the support of the other apps will help you out.

     

    Perhaps he only wants to have a test drive and will come back

    afterwards, convinced that he will stay with what he has  image image  SCNR

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richard_H
    0 Richard_H over 15 years ago

    Am 07.02.2011 23:12, schrieb Joe Adler:

    Does anyone have any suggestions or information about converting PCB or Schematic files from Eagle into other program formats?  Or reading any from any other software into Eagle?

     

     

    Any information related to  Allegro, or Cadstar or Orcad or Pads or P-Cad, or just about any other format would be appreciated.

     

    Thanks

     

     

    Hi

     

    there are different ULPs that allow converting data from EAGLE

    into other formats, like

    eagle2kicad*.ulp -- data for KiCAD PCB suite

    eagle2ad_sch.ulp  -- Generate schematics in Protel / Altium format

    export_cadence_telesis.ulp --      Exports netlist from Eagle to Allegro

     

    For import:

    Netlist in "Protel default" format -- netlist_protel.ulp

    Protel Netlist in EAGLE-Script for layouts -- protel2eagle.zip

    Orcad netlist -- orcad_netlist.ulp

    Tango netlist -- import-tango.ulp

    Orcad schematics -- importbom_and_netlist.zip

    Electronic Workbench data in EAGLE Script for layouts -- ewb2egl.zip

    DDF from Ultiboard PCB  -- import-ultiboard-DDF.ulp

     

    And more..... see Download area, ULP directory

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Joe Adler <jadler54@charter.net> wrote:

    Does anyone have any suggestions or information about converting PCB or

    Schematic files from Eagle into other program formats?  Or reading any

    from any other software into Eagle?

     

     

    Isnt this a bit like asking a VW salesman where you can buy a Volvo?

    Yes, Im sure the support of the other apps will help you out.