Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Modifing package in library isn't changing board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 538 views
  • Users 0 members are here
Related

Modifing package in library isn't changing board

e14 Contributor
e14 Contributor over 14 years ago

I have version 5.11 and have used eagle for years now, recently upgraded our 3 licences and library is some how different.

used to open library, modify package or add a package to existing device, and connect pins between symbol and package then use libarary update from menu, and board would change to new package.

But either i am airhead or there is somthing different about way it's done

 

also under change menu there was option to change package, now instead it has technology but the packages i added aren't showing up either is there a new method I don't understand?

Attachments:
relay.lbr.zip
38811_X.brd.zip
38811_X.sch.zip
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 11/16/2011 01:52 PM, Warren Brayshaw wrote:

    ...

    What seems to be happening now, on occasion, is that the library resets its

    USE setting so the design can't  use your recently modified library.

    Ensure it is USED before the update.

     

    Now that you mention it, this has happened to me several times - a

    library in use gets dropped.  I've always blamed it on some boneheaded

    engineer that dropped it with an errant mouse click.

     

    It seems to surround editing a library and updating it.  I'll have to

    start keeping closer track of exact keystrokes and clicks so Cadsoft can

    duplicate it.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    mark sutliff wrote:

    I have version 5.11 and have used eagle for years now, recently

    upgraded our 3 licences and library is some how different.

    used to open library, modify package or add a package to existing

    device, and connect pins between symbol and package then use libarary

    update from menu, and board would change to new package. But either i

    am airhead or there is somthing different about way it's done

     

    also under change menu there was option to change package, now

    instead it has technology but the packages i added aren't showing up

    either is there a new method I don't understand?

     

    Previously when you opened a library to modify it and then returned to the

    design and performed a "library update/ update all" it worked reliably.

    What seems to be happening now, on occasion, is that the library resets its

    USE setting so the design can't  use your recently modified library.

    Ensure it is USED before the update.

     

    This has happened to me a only a few times but did happen again two days

    ago.

    There have been a few posts recently suggesting this is happening. The trick

    is to view that the library is 'used' prior to the library mods to ensure

    one is clear that this is happening.

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de