Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Wire styles: long dash, short dash, dot dash -- anyone know the repetition algorithm?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 1033 views
  • Users 0 members are here
  • eagle
  • pattern
  • wire
  • dot
  • dash
Related

Wire styles: long dash, short dash, dot dash -- anyone know the repetition algorithm?

e14 Contributor
e14 Contributor over 14 years ago

I've recently acquired an HP plotter. I know there's a ULP script that can generate HPGL, but it's routing, fill,  and pen lift/drop optimization isn't the best.  It can take a LONG to plot a small board.

 

I'm working on a python script that reads the new XML format, and creates an optimized pen path and fill patterns; this could be used for either additive (plotters) or subtractive (routers) creation of a PCB.

 

Anyway, things are going well, and I'm in the implementation phase of the rendering of the polygons.  I would like that the output matches the what's shown in Eagle exactly.  To that end, I'm having a bit of trouble with how Eagle decides to show non-continuous wire patterns.

 

Messing around with a single horizontal wire, it seems that when using the 'long dash' pattern, it begins when the wire reaches a length of 10.5 mm.  Under 10.5, it is a continuous wire. At 10.5, you have two long dashes with a 1.5mm gap.  From there, it adds another long dash every 4mm: 10.5, 14.5, 18.5, 22.5, etc.  The gap is always 1.5mm, and the longdash length is adjusted to fit.  The line always ends on a longdash.

 

For the shortdash, the first one is at 2.01 (not 2.0).

 

Can anyone comment on what rule(s) determine how many repetitions are shown for a given line length.  I can hard-code the rules into the code, but I think there is a simple mathematical rule that I haven't been able to figure out yet.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 12.01.2012 20:03, schrieb Mr.Surly:

    Can anyone comment on what rule(s) determine how many repetitions are shown

     

    You need not care about the rules. EAGLE gives you the partial lines

    free of charge with

       W.pieces()

    (W being an UL_WIRE object).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 12.01.2012 20:03, schrieb Mr.Surly:

    Can anyone comment on what rule(s) determine how many repetitions are shown

     

    You need not care about the rules. EAGLE gives you the partial lines

    free of charge with

       W.pieces()

    (W being an UL_WIRE object).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    You need not care about the rules. EAGLE gives you the partial lines

    free of charge with

       W.pieces()

    (W being an UL_WIRE object).

     

     

    That's true for ULP scripts.  I'm writing a python program that reads the XML file format. The XML save format does not provide the wire pieces.