Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Merging Libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1104 views
  • Users 0 members are here
  • library
  • merge
Related

Merging Libraries

e14 Contributor
e14 Contributor over 14 years ago

Has anyone had any luck with the ULP that dumps and then merges libraries?  I have tried every permutation I can think of and nothing works.  I dumped the contents of the two libraries.  One - Microchip-2.lbr and the other a PIC18F device I created as its own library.  The dump seems to go okay but the merge just won't work.  It says to use the lbr-contents-dump.ulp routine first.  (which of course I did).  I guess I need a few more instructions on how to use this ulp.

Thanks for any help anyone can offer.

Paul

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 25.01.2012 04:32, schrieb Paul Czarapata:

    Has anyone had any luck with the ULP that dumps and then merges libraries?  I have tried every permutation I can think of and nothing works.  I dumped the contents of the two libraries.  One - Microchip-2.lbr and the other a PIC18F device I created as its own library.  The dump seems to go okay but the merge just won't work.  It says to use the lbr-contents-dump.ulp routine first.  (which of course I did).  I guess I need a few more instructions on how to use this ulp.

    Thanks for any help anyone can offer.

    Paul

     

     

    According the description the ulp does what I do with a few mouse

    clicks, so I don't use this ulp.

    If you want to add just a few devices to a target library just open that

    one, go into the control panel (cp), select the devices and right-click

    one by one for a dialog to "copy into the (open) library" (lib).

    Same goes if you make both windows visible (cp & targetlibrary) and just

    drag & drop the device from cp to lib.

    If the amount is larger like merging two libraries, open the source

    library and export the whole lib as a script file:" data /export /script

    (filename)". Then open the target lib:"data /execute script (filename of

    the former scipt)" and the the contents of the other lib is imported.

    No sweat image but try this with copies and a new testlibrary first.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Joem,

    I got it to work but when I opened the part in the merged library it had no pin information on the symbol. I'll give your method a try tonight.

    Thanks,

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 25.01.2012 17:53, schrieb Paul Czarapata:

    Thanks Joem,

    I got it to work but when I opened the part in the merged library it had no pin information on the symbol. I'll give your method a try tonight.

    Thanks,

    Paul

     

     

    So far, so good. I don't know what you mean exactly by "pin

    information". Do you mean the "direction information"- that can be made

    visible switching on the pin layer 93 (display).

    If you mean the pin name and /or the pad number then you must edit the

    symbol of the device in the library by using CHANGE VISIBLE and select

    no/pin/pad/both and apply that on every pin you want to change.

    Since one uses it usually equal for all pins, you group all the pins first.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Paul Czarapata wrote:

    Hello Joem,

    what I meant was when I opened the symbol, all it had was the square

    outling and name. No pin names and no pins. I turned all layers on

    and nothing was there. I wonder if it was because it was a microchip

    part and they have multiple names on the same pin. In any event your

    previous suggestion worked for what I needed. Thanks again,

    Paul

     

     

    Out of interest which version of Eagle are you using?

    Currently I would expect any number of stange occurances with v6. Some due

    to v6 current state and others due to the ULPs , written for an earlier

    version, tripping up in v6.

     

    Warren

     

     

     

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Paul Czarapata wrote:

    Hello Joem,

    what I meant was when I opened the symbol, all it had was the square

    outling and name. No pin names and no pins. I turned all layers on

    and nothing was there. I wonder if it was because it was a microchip

    part and they have multiple names on the same pin. In any event your

    previous suggestion worked for what I needed. Thanks again,

    Paul

     

     

    Out of interest which version of Eagle are you using?

    Currently I would expect any number of stange occurances with v6. Some due

    to v6 current state and others due to the ULPs , written for an earlier

    version, tripping up in v6.

     

    Warren

     

     

     

    Viewed / responded via the newsgroup at

    news.cadsoft.de