EAGLE User Chat (English) What are the setting for the Excellon drill .cam file?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 444 views
  • Users 0 members are here
Related

What are the setting for the Excellon drill .cam file?

Former Member
Former Member over 13 years ago

Hello everyone,

 

I need to know the following:  integer format: 2.3?  2.4? (need 2.4) zero supression (leading, trailing, or none) positioning (absolute or relative).  I know its a .CAM file, but do you set or check the settings?

 

Thanks,

Duane

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    On 06.06.2012 23:20, Duane Brantley wrote:

    Hello everyone,

     

    I need to know the following:  integer format: 2.3?  2.4? (need 2.4) zero supression (leading, trailing, or none) positioning (absolute or relative).  I know its a .CAM file, but do you set or check the settings?

     

    Thanks,

    Duane

     

     

    The EXCELLON device is defined in the eagle.def.

     

     

    Type     = DrillStation

    Long     = "Excellon drill station"

    Init     = "M48\nINCH,LZ,00.0000\n"

    Reset    = "M30\n"

    ResX     = 10000

    ResY     = 10000

    ;Rack     = ""

    DrillSize  = "%sC%0.4f\n"        ; (Tool code, tool size)

    AutoDrill  = "T%02d"             ; (Tool number)

    FirstDrill = 1

    BeginData  = "%%\nM72\nG90\n"

    Units    = Inch

    Select   = "%s\n"                ; (Drill code)

    Drill    = "X%1.0fY%1.0f\n"      ; (x, y)

    Info     = "Drill File Info:\n"\

                "\n"\

                " Data Mode         : Absolute\n"\

                " Units             : 1/10000 Inch\n"\

                "\n"

     

     

     

     

    The data format is 2.4, inch, absolute, LZ (leading zero sup)

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/