Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) problem with connecting net to zg2100-mrf24wb0ma.lbr
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 413 views
  • Users 0 members are here
Related

problem with connecting net to zg2100-mrf24wb0ma.lbr

e14 Contributor
e14 Contributor over 13 years ago

I downloaded the following library:

 

zg2100-mrf24wb0ma.lbr

Library File for the layout of Wifi modules ZG2100MC and RF24WB0MA modules
Uploaded by M Wesseler from Sheffield Hallam University

 

However, when I go to connect a wire to the the part in the library, the wire doesn't end up connected to anything.

 

Simply put:  put a pic microsontroller in schematic, add the mrf24wb0ma module to the schematic, click on net and connect any pin from pic to any pin on mrf24wb0ma module.  The connection doesn't land on anything and going to board layout, the wire is missing.    I can connect any pins from the microcontroller to itself without issue or other parts.

 

Thanks,

Vincent

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks!  I was rooting around in that area but just couldn't make sense of it.  The answer was spot on!  Now to finish my design take over the world.........

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    krobine wrote:

    I downloaded the following library:

     

    zg2100-mrf24wb0ma.lbr

    Library File for the layout of Wifi modules ZG2100MC and RF24WB0MA

    modules

    Uploaded by M Wesseler from Sheffield Hallam University

     

    However, when I go to connect a wire to the the part in the library,

    the wire doesn't end up connected to anything.

     

    Simply put: put a pic microsontroller in schematic, add the

    mrf24wb0ma module to the schematic, click on net and connect any pin

    from pic to any pin on mrf24wb0ma module. The connection doesn't land

    on anything and going to board layout, the wire is missing. I can

    connect any pins from the microcontroller to itself without issue or

    other parts.

     

    Thanks,

    Vincent

     

    The part has not been built on a 0.1" grid as recommended

    It has been built using a 1mm grid and the pins are 2mm apart. No doubt the

    creator has set up all of their environment/libraries this way.

     

    So if you are working with the recommended 0.1" schematic grid then you

    should modify the Library symbol using  a grid of 0.1".

    Move each pin while holding down the CTL key so they snap to the grid

    spacing, you may like to reposition  the other lines and text to make the

    symbol look smart..

    save and then perform a "Library- update all" from the schematic to have the

    schematic come right.

     

    Warren

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer