Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle library TO-5 (8 pin) or 8 pin LED?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 1350 views
  • Users 0 members are here
  • eagle
  • pin
  • library
  • 8
  • to-5
Related

Eagle library TO-5 (8 pin) or 8 pin LED?

e14 Contributor
e14 Contributor over 13 years ago

Hi! I have a create a flex board and a component is an 8 pin TO-5 however I was not able to find a library in eagle does anyone knows where this is available? It's like an 8 pin LED that is round

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Leslie vasquez wrote:

    Hi! I have a create a flex board and a component is an 8 pin TO-5

    however I was not able to find a library in eagle does anyone knows

    where this is available? It's like an 8 pin LED that is round

     

    You may be talking about a TO99 there is one in the ref-packages library.

     

    When making queries like this you should identify the component and obtain

    the datasheet. Confirm from the datasheet the exact package and its

    dimensions and then go looking for that package. Do that by attampting an

    ADD from the board only and search for the package.

     

    HTH

    Warren

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Warren,

     

    thanks for the clarification. I'veincluded the component its a Custom LED and now I have the dimensions. My problem is that I cannot find which library has the component? It is an 8 leg LED under the datasheet packaged is left blank so I am not sure where to look. Thanks for the help!

     

    http://www.epitex.com/products/stem_type_led/pdfs/L4X730-4X805-4X850-40Q96-I.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 11.02.2013 21:57, schrieb Leslie vasquez:

    Hi Warren,

     

    thanks for the clarification. I'veincluded the component its a Custom LED and now I have the dimensions. My problem is that I cannot find which library has the component? It is an 8 leg LED under the datasheet packaged is left blank so I am not sure where to look. Thanks for the help!

     

    http://www.epitex.com/products/stem_type_led/pdfs/L4X730-4X805-4X850-40Q96-I.pdf

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69409#69409/l/re-eagle-library-to-5-8-pin-or-8-pin-led

     

     

    If you can't find the device you have to construct it yourself.

    IMO the TO99 case has the same measures as the TO5, so you could use the

    TO99 case which can be found in the ref-packages.lbr . Copy that package

    into your own library BUT OBSERVE the TO99 has the indicator on pin 8

    while your datasheet shows the lED indicator on pin 1. So you have to

    rename the numbers to fit.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 11.02.2013 21:57, schrieb Leslie vasquez:

    Hi Warren,

     

    thanks for the clarification. I'veincluded the component its a Custom LED and now I have the dimensions. My problem is that I cannot find which library has the component? It is an 8 leg LED under the datasheet packaged is left blank so I am not sure where to look. Thanks for the help!

     

    http://www.epitex.com/products/stem_type_led/pdfs/L4X730-4X805-4X850-40Q96-I.pdf

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69409#69409/l/re-eagle-library-to-5-8-pin-or-8-pin-led

     

     

    If you can't find the device you have to construct it yourself.

    IMO the TO99 case has the same measures as the TO5, so you could use the

    TO99 case which can be found in the ref-packages.lbr . Copy that package

    into your own library BUT OBSERVE the TO99 has the indicator on pin 8

    while your datasheet shows the lED indicator on pin 1. So you have to

    rename the numbers to fit.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag