Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) PCB board for Chip testing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 826 views
  • Users 0 members are here
  • board
  • pads
  • chip
Related

PCB board for Chip testing

e14 Contributor
e14 Contributor over 13 years ago

Hello, I'm starting to work with EAGLE software because i have a project that i have to develop for my university.

 

I have to make a PCB board that will be used to test 4 chips. Each one of this chips has 4 comparators.

 

So my teacher told me to start by creating a part on EAGLE that represents the chip. I created this part in a .lbr file with 12 pins: CLK1, CLK2, CLK3, CLK4, VO1, VO2, VO3, VO4, VDD, VSS, VINP, VINN.

 

When i'm making the symbol, after having the 12 pins, which button should i use for wiring the pins to each other? "Wire" or "Polygon" ?

 

After drawing the symbol i made the package and my teacher told me that the pads should be at a distance of 0.1 mm from each other so i used very tiny pads.

The problem is that if i use a normal resistor with the chip that i just made it looks ridiculous because the resistor if so much bigger. And besides that i don't know which type of pads i should use? The green ones or the red?

Can i change the size of a resistor on eagle?

 

I've attached the library with the chip symbol that i made so that somebody can help me by seeing that mistakes that i possibly did.

 

Thank you

Attachments:
chip4comp_V2.zip
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    You probably need to follow the tutorial, there is a very good user guide. Once you've done that, you'll

    have a much clearer idea of how to proceed.

    Regarding pad sizes, you should follow the guidelines in the manufacturer datasheets. They are optimal.

     

    Regarding colors, they are a little meaningless because they can change depending on user preferences.

    You can refer to this layers reference to get an idea of the concept of layers in EAGLE (I wrote it a while back to

    help myself remember, but you may find it useful).

     

    By default, green is usually for through-hole components, known as Pads in Eagle terminology, or for vias.

    The red is usually used to define the copper for surface mount devices.

    You'll see some examples in that doc.

     

    Basically, the connection mapping between the logical schematic symbol and the physical landing pattern is achieved by

    clicking on the button shown at the top of this picture. It allows you then to add the symbol, etc. Important parts are highlighted here.

    Clicking 'Connect' allows you to perform the mapping.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago

    You probably need to follow the tutorial, there is a very good user guide. Once you've done that, you'll

    have a much clearer idea of how to proceed.

    Regarding pad sizes, you should follow the guidelines in the manufacturer datasheets. They are optimal.

     

    Regarding colors, they are a little meaningless because they can change depending on user preferences.

    You can refer to this layers reference to get an idea of the concept of layers in EAGLE (I wrote it a while back to

    help myself remember, but you may find it useful).

     

    By default, green is usually for through-hole components, known as Pads in Eagle terminology, or for vias.

    The red is usually used to define the copper for surface mount devices.

    You'll see some examples in that doc.

     

    Basically, the connection mapping between the logical schematic symbol and the physical landing pattern is achieved by

    clicking on the button shown at the top of this picture. It allows you then to add the symbol, etc. Important parts are highlighted here.

    Clicking 'Connect' allows you to perform the mapping.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    Thank you for answering, i will try to find some useful info on that guide