Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) PCB board for Chip testing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 830 views
  • Users 0 members are here
  • board
  • pads
  • chip
Related

PCB board for Chip testing

e14 Contributor
e14 Contributor over 13 years ago

Hello, I'm starting to work with EAGLE software because i have a project that i have to develop for my university.

 

I have to make a PCB board that will be used to test 4 chips. Each one of this chips has 4 comparators.

 

So my teacher told me to start by creating a part on EAGLE that represents the chip. I created this part in a .lbr file with 12 pins: CLK1, CLK2, CLK3, CLK4, VO1, VO2, VO3, VO4, VDD, VSS, VINP, VINN.

 

When i'm making the symbol, after having the 12 pins, which button should i use for wiring the pins to each other? "Wire" or "Polygon" ?

 

After drawing the symbol i made the package and my teacher told me that the pads should be at a distance of 0.1 mm from each other so i used very tiny pads.

The problem is that if i use a normal resistor with the chip that i just made it looks ridiculous because the resistor if so much bigger. And besides that i don't know which type of pads i should use? The green ones or the red?

Can i change the size of a resistor on eagle?

 

I've attached the library with the chip symbol that i made so that somebody can help me by seeing that mistakes that i possibly did.

 

Thank you

Attachments:
chip4comp_V2.zip
  • Sign in to reply
  • Cancel
Parents
  • andrewk182
    0 andrewk182 over 13 years ago

    red pad's , yes you can the size that I know of image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • andrewk182
    0 andrewk182 over 13 years ago

    red pad's , yes you can the size that I know of image