Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) pcb, gerber&drill files problem
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1829 views
  • Users 0 members are here
Related

pcb, gerber&drill files problem

e14 Contributor
e14 Contributor over 13 years ago

Hi there,

 

I'm ready to send my first board to a pcb manufacturer. I've generated the GBL,GTL,GBS,GTS,GBO,GTO and the drill TXT file using the manufacturer's cam.

Now the problem is that when I open those files with two separate gerber viewers (GERBV 2.6 and Viewplot) I get the same result.. the holes are where they're supposed to, but everything else is placed +0.409 mm from the origin, on both axes.

It took me a while to understand what's wrong, and after that I placed everything in Eagle's Board Editor 0.409 mm right from and 0.409 mm above the origin. After that I generated a new set of gerber/drill files and the problem seemed to be solved. I mean I get the same exact (positive) results in two different gerber viewers.

 

My questions is why is that happening, if it's normal (like an alignment of the board from 0.409,0.409 and not from 0,0) and if should send it like that.

Can I trust these software viewer that the board would look exactly like that when finished ?

 

what's bother me the most is that in the second scenario the holes are still at the same coordinates and only the other layers were repositioned (although I selected and moved everything in eagle).

 

thanks in advance

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 13 years ago

    On 5/3/2013 7:44 PM, Jim Raynor wrote:

    Hi there,

     

    I'm ready to send my first board to a pcb manufacturer. I've generated

    the GBL,GTL,GBS,GTS,GBO,GTO and the drill TXT file using the

    manufacturer's cam.

    Now the problem is that when I open those files with two separate gerber

    viewers (GERBV 2.6 and Viewplot) I get the same result.. the holes are

    where they're supposed to, but everything else is placed +0.409 mm from

    the origin, on both axes.

    It took me a while to understand what's wrong, and after that I placed

    everything in Eagle's Board Editor 0.409 mm right from and 0.409 mm

    above the origin. After that I generated a new set of gerber/drill files

    and the problem seemed to be solved. I mean I get the same exact

    (positive) results in two different gerber viewers.

     

    My questions is why is that happening, if it's normal (like an alignment

    of the board from 0.409,0.409 and not from 0,0) and if should send it

    like that.

    Can I trust these software viewer that the board would look exactly like

    that when finished ?

     

    what's bother me the most is that in the second scenario the holes are

    still at the same coordinates and only the other layers were

    repositioned (although I selected and moved everything in eagle).

     

    thanks in advance

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/75600#75600

     

     

    Hi Jim,

     

    The key here is the pos. coords option needs to be set the same across

    all of the gerber tabs and drill job. Either have them all set or have

    them unset but you can't have a mix. You don't have to make any changes

    to the board design for this to work.

     

    If pos. coords is checked across all of the tabs then all of the design

    files will have the same offset added to them so everything will line up

    nicely.

     

    hth,

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to autodeskguest

    Am 07.05.2013 21:14, schrieb Jorge Garcia:

    The key here is the pos. coords option needs to be set the same across

    all of the gerber tabs and drill job. Either have them all set or have

    them unset but you can't have a mix.

     

    Fine to see that there is a possibility to make this work properly in EAGLE.

     

    BUT since this is not obvious, why leave the user in the dark about it?

    If "pos. coords" should be either on or off in ALL the CAM tabs, why not

      1. either make this option GLOBAL for the whole job (so as not to give

         the user the chance to screw things up),

      2. or leave it as it is, but, in case the user checked the option in

         SOME tabs, but not in others, display a warning that this MIGHT

         cause problems with the Gerber output?

    If a software gives the user vital information on how NOT to do things,

    or prevents him from doing these wrong things, that's MUCH better than

    letting him run against the wall...

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to autodeskguest

    On 5/8/2013 4:31 AM, Andreas Weidner wrote:

    Am 07.05.2013 21:14, schrieb Jorge Garcia:

    The key here is the pos. coords option needs to be set the same across

    all of the gerber tabs and drill job. Either have them all set or have

    them unset but you can't have a mix.

     

    Fine to see that there is a possibility to make this work properly in

    EAGLE.

     

    BUT since this is not obvious, why leave the user in the dark about it?

    If "pos. coords" should be either on or off in ALL the CAM tabs, why not

      1. either make this option GLOBAL for the whole job (so as not to give

         the user the chance to screw things up),

      2. or leave it as it is, but, in case the user checked the option in

         SOME tabs, but not in others, display a warning that this MIGHT

         cause problems with the Gerber output?

    Hi Andreas,

     

    I like number 2, I'll file an enhancement report on this. I don't think

    it would be difficult to implement so thanks for the idea.

     

    Best Regards,

    Jorge Garcia

    If a software gives the user vital information on how NOT to do things,

    or prevents him from doing these wrong things, that's MUCH better than

    letting him run against the wall...

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to autodeskguest

    On 5/8/2013 4:31 AM, Andreas Weidner wrote:

    Am 07.05.2013 21:14, schrieb Jorge Garcia:

    The key here is the pos. coords option needs to be set the same across

    all of the gerber tabs and drill job. Either have them all set or have

    them unset but you can't have a mix.

     

    Fine to see that there is a possibility to make this work properly in

    EAGLE.

     

    BUT since this is not obvious, why leave the user in the dark about it?

    If "pos. coords" should be either on or off in ALL the CAM tabs, why not

      1. either make this option GLOBAL for the whole job (so as not to give

         the user the chance to screw things up),

      2. or leave it as it is, but, in case the user checked the option in

         SOME tabs, but not in others, display a warning that this MIGHT

         cause problems with the Gerber output?

    Hi Andreas,

     

    I like number 2, I'll file an enhancement report on this. I don't think

    it would be difficult to implement so thanks for the idea.

     

    Best Regards,

    Jorge Garcia

    If a software gives the user vital information on how NOT to do things,

    or prevents him from doing these wrong things, that's MUCH better than

    letting him run against the wall...

     

    Andreas Weidner