Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Beginners PinHead library question
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1641 views
  • Users 0 members are here
Related

Beginners PinHead library question

donrecardo
donrecardo over 12 years ago

Hi

I need to place 12 pinhead connectors in a 4 x 3 matrix with 0.1 inch between pins in each direction

 

I thought it might be simple just place three 1x4 pinhead parts in rows with each row 1/10th of an inch apart

but I tried that and the pads on the 1 x 4 are so big that each row overlaps the next

 

If I only wanted 8 pins in two rows of 4 it would be fine because the 2x4 pinhead part has much smaller pads

I am guessing I am going to need to modify the library to make the pads on the 1x4 part smaller, just like on the 2x4

Can somebody walk me through the process please of how to change the pads in a way a beginner would understand

 

Regards

Don

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    Am 12.03.2014 20:35, schrieb Don Recardo:

    Hi

    I need to place 12 pinhead connectors in a 4 x 3 matrix with 0.1 inch

    between pins in each direction

     

    I thought it might be simple just place three 1x4 pinhead parts in rows

    with each row 1/10th of an inch apart

    but I tried that and the pads on the 1 x 4 are so big that each row

    overlaps the next

     

    If I only wanted 8 pins in two rows of 4 it would be fine because the

    2x4 pinhead part has much smaller pads

    I am guessing I am going to need to modify the library to make the pads

    on the 1x4 part smaller, just like on the 2x4

    Can somebody walk me through the process please of how to change the

    pads in a way a beginner would understand

     

    Regards

    Don

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/106092

     

     

    You mean that the pads are to big in the board or the library?

    You didn't mention it.

    Check the library. If the pads are ok for you and they are only too big

    in your board then check the restring settings in your design rules (DRC).

    If the pads are too big in the library already then copy that part or

    the library into a new library and edit the part THERE.

    Do not edit the eagle libraries.

    And it would be better for understanding if you mention the part and the

    library name next time.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • donrecardo
    0 donrecardo over 12 years ago in reply to autodeskguest

    Hi Joern and thanks for the reply

     

    I will try to rephrase my question better and give the information you needed that I missed off.

     

    The Library that the parts are in is called pinhead

    The part I am trying to use is called  PINHD-1X4

     

    It is a strip of 4 pin connectors in a line with 0.1 inch between pins

     

    There is a similar part in the same library and its called PINHD-2X4

    This part is two strips of 4 pins side by side ,

     

    Now if you go to the library and click on each of those parts and look at the picture of its package

    you will see the PINHD-2X4 has small round pads  but the PINHD-1X4 has large oval pads .

    The pads are so large that if I place two of the PINHD-1X4 parallel to each other with 0.1 inch between the parts

    so that it looks like the PINHD-2X4 part then the pads are so big they overlap each other

    This is a problem because I need to place 3 pieces of the PINHD-1X4 together to make what would be  I suppose a PINHD-3X4 if it existed

     

    So yes you are right  What I need to do is take a copy of the PINHD-1X4 and modify it to have the same size pads as the PINHD-2X4

    and that is what I was trying to say in my post 

    Can anyone give me a step by step explanation of how I do this , explained in a ,open this, click that , choose this type of format that even

    a beginner like me can follow.

     

    Hope someone can help

     

    Don 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • donrecardo
    0 donrecardo over 12 years ago in reply to autodeskguest

    Hi Joern and thanks for the reply

     

    I will try to rephrase my question better and give the information you needed that I missed off.

     

    The Library that the parts are in is called pinhead

    The part I am trying to use is called  PINHD-1X4

     

    It is a strip of 4 pin connectors in a line with 0.1 inch between pins

     

    There is a similar part in the same library and its called PINHD-2X4

    This part is two strips of 4 pins side by side ,

     

    Now if you go to the library and click on each of those parts and look at the picture of its package

    you will see the PINHD-2X4 has small round pads  but the PINHD-1X4 has large oval pads .

    The pads are so large that if I place two of the PINHD-1X4 parallel to each other with 0.1 inch between the parts

    so that it looks like the PINHD-2X4 part then the pads are so big they overlap each other

    This is a problem because I need to place 3 pieces of the PINHD-1X4 together to make what would be  I suppose a PINHD-3X4 if it existed

     

    So yes you are right  What I need to do is take a copy of the PINHD-1X4 and modify it to have the same size pads as the PINHD-2X4

    and that is what I was trying to say in my post 

    Can anyone give me a step by step explanation of how I do this , explained in a ,open this, click that , choose this type of format that even

    a beginner like me can follow.

     

    Hope someone can help

     

    Don