Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Pads and Nets both red, so I'm a little confused.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 979 views
  • Users 0 members are here
  • eagle
  • pads
  • nets
Related

Pads and Nets both red, so I'm a little confused.

e14 Contributor
e14 Contributor over 12 years ago

I made a simple PCB that involves surface mounting large components (.15x.076 pads), and noticed that both the pads and net connections are all red in the Board Editor.  I just wanted to make sure that this is ok, and that the pads are actually above the surface for soldering, and the net connections are non-exposed inside the board.  Silly question I know, but just wanted to make sure before paying for the PCB.  (this would be my second pcb, but the last one was like 6 years ago so I'm rusty). 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    On 04/21/2014 01:10 PM, David Henry wrote:

    I made a simple PCB that involves surface mounting large components

    (.15x.076 pads), and noticed that both the pads and net connections are

    all red in the Board Editor.  I just wanted to make sure that this is

    ok, and that the pads are actually above the surface for soldering, and

    the net connections are non-exposed inside the board.  Silly question I

    know, but just wanted to make sure before paying for the PCB.  (this

    would be my second pcb, but the last one was like 6 years ago so I'm

    rusty). 

     

    David,

     

    Unless you've changed the default colors, red represent copper on the

    top layer (layer 1).  If you mirror the package on the board, the pads

    will turn blue indicating that they're on the bottom copper layer (layer

    16).

     

    You can turn on the tStop layer to see where the solder mask has been

    pulled back from the pad.  This area should be slightly larger than the

    copper pad.  You can also turn on the tCream layer which indicates where

    solder paste should be applied.  It should be slightly smaller than the

    pad itself.

     

    As a verification step, I display the gerber files produced by the CAM

    Processor in a viewer like gerbv.  The source code is available on

    SourceForge as is a binary for Win32.

     

    There are also a handful of associated programs available from gerbv's

    home page at http://gerbv.geda-project.org/ .

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 12 years ago

    On 04/21/2014 01:10 PM, David Henry wrote:

    I made a simple PCB that involves surface mounting large components

    (.15x.076 pads), and noticed that both the pads and net connections are

    all red in the Board Editor.  I just wanted to make sure that this is

    ok, and that the pads are actually above the surface for soldering, and

    the net connections are non-exposed inside the board.  Silly question I

    know, but just wanted to make sure before paying for the PCB.  (this

    would be my second pcb, but the last one was like 6 years ago so I'm

    rusty). 

     

    David,

     

    Unless you've changed the default colors, red represent copper on the

    top layer (layer 1).  If you mirror the package on the board, the pads

    will turn blue indicating that they're on the bottom copper layer (layer

    16).

     

    You can turn on the tStop layer to see where the solder mask has been

    pulled back from the pad.  This area should be slightly larger than the

    copper pad.  You can also turn on the tCream layer which indicates where

    solder paste should be applied.  It should be slightly smaller than the

    pad itself.

     

    As a verification step, I display the gerber files produced by the CAM

    Processor in a viewer like gerbv.  The source code is available on

    SourceForge as is a binary for Win32.

     

    There are also a handful of associated programs available from gerbv's

    home page at http://gerbv.geda-project.org/ .

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dukepro

    Chuck, I turned on tStop and tCream and all looks well.  I'm surprised those layers aren't on by default.  I'll also try to figure out Gerbv.  Really appreciate it  Thanks.