Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) >$1000 for a simple 8"x8" PCB???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 192 subscribers
  • Views 1961 views
  • Users 0 members are here
  • eagle
  • pcb
Related

>$1000 for a simple 8"x8" PCB???

e14 Contributor
e14 Contributor over 12 years ago

I want to make a simple PCB, so I'm looking at Eagle as it seems to be what other hobbiests use.

The board is 8" x 8", and will have only a few LEDs and chip resistors on it. I don't need multiple layers, libraries, autorouting, or even drilled holes. I could make the PCB by hand with a utility knife, but I thought using a PCB program would be neater and cause less hand stress. BUT it seems the Eagle program is more than $1000 to do this! Do other hobbiests really spend this? (I was hoping for free...)

My question: Is there another program out there cheaper, Eagle just seems unreasonably priced.

  • Sign in to reply
  • Cancel
Parents
  • vsluiter
    0 vsluiter over 12 years ago

    Hi Steve,

     

    At work I'm using a design package that costs 1k anually for maintenance... It does however work very well, with very little frustration during routing.

    For private projects I used to work with Eagle, but as I got more and more fed up with the illogical way it is routing (no live DRC, no dynamic routing, no way to easily shift segments while keeping 45 degree angles) I recently migrated to KiCad. It has its quirks, and a very limited amount of DRC rules, but it works, and is more consistent in operation than Eagle if you ask me. Anyway, I don't want to start a tool-war, just saying that a free alternative exists!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago

    Hi Steve,

     

    At work I'm using a design package that costs 1k anually for maintenance... It does however work very well, with very little frustration during routing.

    For private projects I used to work with Eagle, but as I got more and more fed up with the illogical way it is routing (no live DRC, no dynamic routing, no way to easily shift segments while keeping 45 degree angles) I recently migrated to KiCad. It has its quirks, and a very limited amount of DRC rules, but it works, and is more consistent in operation than Eagle if you ask me. Anyway, I don't want to start a tool-war, just saying that a free alternative exists!