Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) >$1000 for a simple 8"x8" PCB???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 192 subscribers
  • Views 1961 views
  • Users 0 members are here
  • eagle
  • pcb
Related

>$1000 for a simple 8"x8" PCB???

e14 Contributor
e14 Contributor over 12 years ago

I want to make a simple PCB, so I'm looking at Eagle as it seems to be what other hobbiests use.

The board is 8" x 8", and will have only a few LEDs and chip resistors on it. I don't need multiple layers, libraries, autorouting, or even drilled holes. I could make the PCB by hand with a utility knife, but I thought using a PCB program would be neater and cause less hand stress. BUT it seems the Eagle program is more than $1000 to do this! Do other hobbiests really spend this? (I was hoping for free...)

My question: Is there another program out there cheaper, Eagle just seems unreasonably priced.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 12 years ago

    Hi Steve you have obviously exceeded the limitations of the Free Eagle (I never remember what they are).

    If I remember right it was something like 100x100mm which is 1/4 of the size you mention. Best idea would be to

    reduce the size of your board but not knowing how dense your board is it may not be practical even if it's not complicated.

    You could however try designing the board in 4 parts then stitching them together using some graphics  package presuming you are

    going to etch this board your self. Failing that you can look on the net Google is your friend here for Free PCB tools or look to see what

    folk are using on sites such as Hackaday or what ever.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Problemchild

    I agree with John,

    Unless there is some demand of form over function; the area needed to perform "only a few LEDs and chip resistors" does not require 8"x8" space. Free Eagle is capable of up to ~100mm if i remember correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Problemchild

    I agree with John,

    Unless there is some demand of form over function; the area needed to perform "only a few LEDs and chip resistors" does not require 8"x8" space. Free Eagle is capable of up to ~100mm if i remember correctly.