Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Does the library editor tool lock a file while editing it?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 1104 views
  • Users 0 members are here
Related

Does the library editor tool lock a file while editing it?

e14 Contributor
e14 Contributor over 12 years ago

I am working in a git controlled evnvironment with several other engineers. Currently we each have a local copy of our libraries that are sync'd through git. The problem of merging libraries files after a Git pull is becoming excessive.

 

We'd like to store all files in a folder on an NFS server accessable by all users. The libraries would still be version controlled by git, with a periodic commits. When an engineer is editing a library, the file is read only to all other users. the other users can view but not concurrently edit the file.

 

does the eagle library editor tool lock open files?

 

If not, is it possible to easily integrate this feature? without any other version controll or check-out software.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 5/13/2014 3:05 PM, Jesse Banks wrote:

    I am working in a git controlled evnvironment with several other

    engineers. Currently we each have a local copy of our libraries that are

    sync'd through git. The problem of merging libraries files after a Git

    pull is becoming excessive.

     

    We'd like to store all files in a folder on an NFS server accessable by

    all users. The libraries would still be version controlled by git, with

    a periodic commits. When an engineer is editing a library, the file is

    read only to all other users. the other users can view but not

    concurrently edit the file.

     

    does the eagle library editor tool lock open files?

     

    Hi Jesse,

     

    EAGLE does not lock open files. Other version control systems have this

    feature and every setup is different. I'm suprised that Git doesn't

    support this as comprehensive a tool as it is.

     

    There are no immediate plans to implement such a feature and

    historically that is something we have left to the VCS.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Why is this not a useful feature? Having eagle elements properly opening and locking active files seems like a useful feature.

     

    I ask this because it seems like the VCS has no idea what any other software is doing with the file. If the shecmatic editor looks into library X, does the VCS realise this is a read only action? Whereas the library editor tool will likely make changes to the file, so it should be locked. how does VCS determine the actions of the software, if not from that software as it opens the file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Why is this not a useful feature? Having eagle elements properly opening and locking active files seems like a useful feature.

     

    I ask this because it seems like the VCS has no idea what any other software is doing with the file. If the shecmatic editor looks into library X, does the VCS realise this is a read only action? Whereas the library editor tool will likely make changes to the file, so it should be locked. how does VCS determine the actions of the software, if not from that software as it opens the file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to e14 Contributor

    On 13/05/14 21:51, Jesse Banks wrote:

    Why is this not a useful feature? Having eagle elements properly opening

    and locking active files seems like a useful feature.

     

    It may, or may not, be useful. Many programs do attempt to use file

    locking (MS Word and OpenOffice for example) to avoid conflicts. The

    result is often that annoying false positives get in the way. I've

    certainly had a lot of annoyance with ooffice refusing to open files on

    network drives because the NFS lock protocol was being iffy.

     

    I ask this because it seems like the VCS has no idea what any other

    software is doing with the file. If the shecmatic editor looks into

    library X, does the VCS realise this is a read only action? Whereas the

    library editor tool will likely make changes to the file, so it should

    be locked. how does VCS determine the actions of the software, if not

    from that software as it opens the file?

     

    The philosophy behind VCS doesn't assume sharing of working files.

    Indeed it makes exactly the opposite assumption - everyone on the team

    WILL have their own local working copy, so that interim versions they

    are experimenting with don't cause other people problems. These working

    copies are kept separate and protected or merged as required. This is a

    fundamentally good way to work, and cannot be handled by any application

    other than the VCS.

     

    Now there are two options for handling the situation where multiple

    people want to work on the same file. Either they are all allowed to

    modify their local copy and the changes are then merged (the default GIT

    approach) or the repository copy is the master and all working copies

    are forced to be read-only unless an explicit "repository lock" is

    obtained. This function cannot be done by anything other than the VCS.

     

    In general, file locking by every application on the system so that all

    files can be shared, is a nasty hack that copes only with a very small

    team who aren't controlling their data at all well. Relying on a VCS to

    perform working copy management is a far better approach.