Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) SOT223; Joining pad to tab
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2635 views
  • Users 0 members are here
  • sot223
Related

SOT223; Joining pad to tab

e14 Contributor
e14 Contributor over 11 years ago

Hi folks.

 

I'm having a problem with using the tab on SOT223 voltage regulators that use the tab as a heatsink and is usually the same connection as the centre pin. But when I add a  polygon around it to increase the surface area, it either leaves the centre pin disconnected or the tab is isolated.

 

Is there a nice way to achieve this?

 

Thank you.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've tried this, but it does not work. It does work with other components, but not this type for some reason.

     

    There seems to be only 3 connections allowed on this 4 connection component. I would rather there be 4, even if it means a messy schematic, as this is mainly a board design program. I would rather have to link the tab on the schematic manually to one of the pins to match the component needed.

     

    Can I edit the component to add this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Name the poly the same name network connected to that pad has. Via naming button, not via info window.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<