Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) SOT223; Joining pad to tab
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 2668 views
  • Users 0 members are here
  • sot223
Related

SOT223; Joining pad to tab

e14 Contributor
e14 Contributor over 11 years ago

Hi folks.

 

I'm having a problem with using the tab on SOT223 voltage regulators that use the tab as a heatsink and is usually the same connection as the centre pin. But when I add a  polygon around it to increase the surface area, it either leaves the centre pin disconnected or the tab is isolated.

 

Is there a nice way to achieve this?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Name the poly the same name network connected to that pad has. Via naming button, not via info window.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've tried this, but it does not work. It does work with other components, but not this type for some reason.

     

    There seems to be only 3 connections allowed on this 4 connection component. I would rather there be 4, even if it means a messy schematic, as this is mainly a board design program. I would rather have to link the tab on the schematic manually to one of the pins to match the component needed.

     

    Can I edit the component to add this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've tried this, but it does not work. It does work with other components, but not this type for some reason.

     

    There seems to be only 3 connections allowed on this 4 connection component. I would rather there be 4, even if it means a messy schematic, as this is mainly a board design program. I would rather have to link the tab on the schematic manually to one of the pins to match the component needed.

     

    Can I edit the component to add this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hpvoelpel
    0 hpvoelpel over 11 years ago in reply to e14 Contributor

    Am 14.12.2014 um 12:39 schrieb Richard Perkins.:

    I have tried other components with this method and it seems simple with

    those, but I'm sure I was trying the same thing with the two I

    mentioned, and it just wasn't working. The main difference I see is that

    the others have the tab numbered 4, so if this is present, then there is

    no problem. The problem seems to start when the tab is not numbered.

    Maybe I just found an awkward couple. If you want to check other sot223

    devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding

    helpful people, and I am still a novice with Eagle, so I expect I will

    be back with more dumb questions.:^0

     

    Thank you all for your help.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/134754

     

     

    PADs are what you see in the board and in the packages, PINs are what

    you see in the schematic and the symbols. You can connect multiple PADs

    to one PIN. This will solve your problem. It has to be done in zthe LBR

    editor. If you want to have a heatsink copper area around a PAD without

    thermals, just draw a polygon in the board and give it the same name as

    the signal the PAD is connected to, and uncheck 'Thermals'. You will see

    the checkbox by activating 'INFO' and clicking on the poly.

    Ever tried 'help connect', 'help poly' etc?

    And, after all, it would be a really good idea to read the manual...

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    I have tried other components with this method and it seems simple with those, but I'm sure I was trying the same thing with the two I mentioned, and it just wasn't working. The main difference I see is that the others have the tab numbered 4, so if this is present, then there is no problem. The problem seems to start when the tab is not numbered. Maybe I just found an awkward couple. If you want to check other sot223 devices to find one without that number 4 tab, and try connecting to it.

     

    Well I have learned a lot more by confronting a problem and finding helpful people, and I am still a novice with Eagle, so I expect I will be back with more dumb questions.image

     

    Thank you all for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to e14 Contributor

    On 14/12/2014 12:51 p.m., Richard Perkins. wrote:

    In the example you gave, there was no electrical connection to the tab.

     

    That's correct in so much as you cannot start routing from the centre of

    the tab as it is not a SMD pad. The whole pad is the tab and the pad #2.

    The only origin for the tab/pad is the origin of the pad so you start

    routing from there, and go straight up to the tab. You can stop there if

    you like or continue routing out of the tab. At any time you can attach

    another route to this initial one by holding CTL and click to start

    routing at any point on a routed wire.

     

    Have a look at (pull apart) the attached board. A resistor to ground on

    each of the pins. Polygons have ranks.  It does not have DRC errors.

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to autodeskguest

    In the example you gave, there was no electrical connection to the tab. On the examples I gave I couldn't even click or select the pad, as although it had a board pad, putting anything on it created an overlap error. Mine have the pins numbered 1,2,3 & 4 now. If I could do it your way, I would. Tried it, but it didn't work for these two components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to e14 Contributor

    On 14/12/2014 2:24 a.m., Richard Perkins. wrote:

    I've found someone else had this problem 6 years ago !!! Is this still

    unresolved ? - How to avoid isolation around a SOT223 collector tab?

    (http://eagle.support.eng.narkive.com/GjWTMXjy/how-to-avoid-isolation-around-a-sot223-collector-tab)

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/134705

     

    This is not a problem with Eagle these days,

    See HELP> Arbitrary Pad Shapes

     

    See the attached. Here I have elected to do away with the SMD for the

    tab pad and draw a polygon on the top layer (coloured green so it stands

    out). The polygon surrounds the origin of the center pin so is

    considered part of it. Thus we have an arbitrary pad shape.

     

    So now you only need three pins for in the schematic symbol that are

    connected to the three pins of the package.

     

    When used in the Board editor there are a couple of precautions

    dependant on your layout.

     

    The thermals for the centre pin will be extended from the SMD origin so

    this will result in only one thermal bridge which will not be enough. In

    this case route up from the center pin to the tab and out from there

    into the polygon area (three route wires in a 'T' shape) At the top of

    the 'T' change the width of the wires to get the desired result.

     

    Alternately turn of thermals for the centre pin in the library  and

    manage the thermal connection with the polygon shape of the heat sink area.

     

    HTH

    Warren

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to dougw

    Thank you for your help. I have finally solved it !

     

    As you say, I've edited the part after finding it in the library and added a pin which was the easy part.  What I had to do then was to "connect" it which was a little complicated and took me a while to find out how.  I saw a "Connect" tab in the lower right window but I've forgotten how I got there. Anyway, this shows you the pins and pad connections. I got confused with the centre panel, as anything in there got added to the top right panel, sometimes with a link symbol, and sometimes a broken link symbol. I'm sure I can find out why eventually, but I did manage to get 4 pins connected to 4 pads, and got a green tick. After saving, this was easy to replace the part I had  - and gave me that extra connection on the schematic. When this was connected, I got an airwire on the board which was correct. Clicking ratsnest filled it in as my ground around the pad with no gaps!

     

    So happy.image

     

    One wrinkle is the pin is given a name which I couldn't see a way to edit that at the time, but maybe it is easy to re-name it before I placed it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago in reply to e14 Contributor

    You are right, the schematic symbol should have a pin for each pin on the device. You can edit the device to add the pin. You could check the 78L05F device in the Linear library to see how they did it there in the SOT89, but note they connected the 2 pins in the device package.

    The LD117AS12TR device in the V-Reg library has an unconnected pad, you can just add a pin to the symbol and connect it in the device window, or create a new symbol with 4 pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I've found someone else had this problem 6 years ago !!! Is this still unresolved ? - How to avoid isolation around a SOT223 collector tab?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Part no. is LD117AS12TR and is a SOT223 in library V-reg.

    This one only allows the tab to be connected, but doesn't like the centre leg being attached to the tab. I'm actually using an LM1117 adj one and the datasheet shows this as the tab is the same as the centre leg.

     

    The other problem I had was another SOT223, part no. NDT2995 and is in the zetex library. This is the one I can't attach anything to the tab. Again datasheet shows the tab is the same as the centre leg.

     

    Both give an overlap error if I try.

     

    Thank you for your time investigating it. If there is an alternative part I can replace these with that will allow a neat board using the sot223 then I might be able to do it this way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Which voltage regulator? Tell me how it is called and in what library it is, I'll investigate