Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) New Library Items Unable to Move Values
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 188 subscribers
  • Views 2527 views
  • Users 0 members are here
Related

New Library Items Unable to Move Values

slk001
slk001 over 10 years ago

I have been using Eagle for over 20 years.  I started with the DOS 3.1 version.  I usually build all my parts from scratch.  My .LBR was started back in the beginning.  When I build a part using versions > 6.3, I am no longer able to SMASH a part and move the VALUE around.  In the image below, C21 and R14 are old parts, being created early in my Eagle days.  They both are SMASHed and they both have the ability to move the NAMES and VALUES around.  U7 and U8 are new parts, both created in 6.5 and both SMASHed, but only the NAMES are able to be moved - the VALUES don't have the "+" handle to grab.

 

One thing that I have changed is the ALIGN from the default value to CENTER.  Changing back to the default "LEFT-BOTTOM" acts the same way.  If I change the VALUE to >VALUE and add the value in the schematic, the value never shows (VALUES layer is ON).

 

I though that I knew Eagle quite well.  This is perplexing me.

 

Does anyone have any ideas?

 

 

image

  • Sign in to reply
  • Cancel
Parents
  • slk001
    slk001 over 10 years ago

    Well, it turns out that I was wrong.  I fired up V3.51 and tried to move a part with the value filled in at the sym level.  When inserted into a schematic and smashed, only the NAME was moveable - the value was not.  To get it to move, I had to fill the value with >VALUE, then enter the correct part value while in the schematic.  Only then was it moveable upon smashing.

     

    My original thinking was that the value didn't change, so why not enter it into the symbol?  If you place it correctly, it usually isn't a problem.  But sometimes it is, so it is back to assigning the >VALUE attribute at the symbol level.

     

    My question to the CadSoft developers, is why isn't this moveable?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to slk001

    On 02.06.2016 23:34, Steve Kersten wrote:

    Well, it turns out that I was wrong.  I fired up V3.51 and tried to move a part with the value filled in at the sym level.  When inserted into a schematic and smashed, only the NAME was moveable - the value was not.  To get it to move, I had to fill the value with >VALUE, then enter the correct part value while in the schematic.  Only then was it moveable upon smashing.

     

    My original thinking was that the value didn't change, so why not enter it into the symbol?  If you place it correctly, it usually isn't a problem.  But sometimes it is, so it is back to assigning the >VALUE attribute at the symbol level.

     

    My question to the CadSoft developers, is why isn't this moveable?

     

     

    Right now, only attributes for value and name are smashable. The

    alternativeis to be able to move every text on value and name layers.

    Ok, I guess it could work since you usually only have one text there,

    but there may be exceptions.

     

    Also the value of the value attribyte is that it will follow package and

    technology selected at the board.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to slk001

    On 02.06.2016 23:34, Steve Kersten wrote:

    Well, it turns out that I was wrong.  I fired up V3.51 and tried to move a part with the value filled in at the sym level.  When inserted into a schematic and smashed, only the NAME was moveable - the value was not.  To get it to move, I had to fill the value with >VALUE, then enter the correct part value while in the schematic.  Only then was it moveable upon smashing.

     

    My original thinking was that the value didn't change, so why not enter it into the symbol?  If you place it correctly, it usually isn't a problem.  But sometimes it is, so it is back to assigning the >VALUE attribute at the symbol level.

     

    My question to the CadSoft developers, is why isn't this moveable?

     

     

    Right now, only attributes for value and name are smashable. The

    alternativeis to be able to move every text on value and name layers.

    Ok, I guess it could work since you usually only have one text there,

    but there may be exceptions.

     

    Also the value of the value attribyte is that it will follow package and

    technology selected at the board.