EAGLE User Support (English) How to add 0R 1206 Resistor as Jumper t o Board Layout
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
  • Replies 15 replies
  • Subscribers 180 subscribers
  • Views 2668 views
  • Users 0 members are here
Related

How to add 0R 1206 Resistor as Jumper t o Board Layout

Former Member
Former Member over 15 years ago

Hi;

Most of the Cad editors allow to add a 0R Resistor to board as a jumper.

But I can't find how to do it without adding to schematic.

 

Thanks in advance..

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 15 years ago

    farabiahmed wrote on Wed, 09 June 2010 11:06

    But I can't find how to do it by Eagle without adding to schematic.

     

    Good, because such things should be in the schematic.  You can make a

    jumper device and have it use your 0 Ohm resistor footprint if you like.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 6/9/2010 2:39 PM, Olin Lathrop wrote:

    farabiahmed wrote on Wed, 09 June 2010 11:06

    >> But I can't find how to do it by Eagle without adding to schematic.

    >

    Good, because such things should be in the schematic. You can make a

    jumper device and have it use your 0 Ohm resistor footprint if you like.

     

    Just curious, what is the rationale to have such in the schematic? I

    could understand if it is a jumper in the sense of selecting a

    particular option. And of course, it needs to be in the BOM no matter what.

     

    But what if the board has a significant jumper layer and there are many

    0R jumpers that are just part of the circuitry, not selecting anything.

    Why would I want to see these on the schematic? How does EAGLE know that

    the net name should be the same on both sides of the jumper?

     

    Is it more expensive to move up from a 2 layer to 4 layer board or just

    add 10 0R jumpers? Looking at real circuit boards from disk drives and

    the like, I see many examples of 2 layer + jumper construction...

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Gary Gofstein schrieb:

     

    Is it more expensive to move up from a 2 layer to 4 layer board or just

    add 10 0R jumpers? Looking at real circuit boards from disk drives and

    the like, I see many examples of 2 layer + jumper construction...

     

    In most cases, a four layer board is significantly more expensive than a

    two layer board with /many/ additional jumpers (depends on board size,

    of course).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On Thu, 10 Jun 2010, Gary Gofstein wrote to us saying :

    >But what if the board has a significant jumper layer and there are many

    >0R jumpers that are just part of the circuitry, not selecting anything.

    >Why would I want to see these on the schematic? How does EAGLE know

    >that the net name should be the same on both sides of the jumper?

     

    Ask yourself why the jumpers are there. Remember, the schematic is the

    master definition, the board is merely an implementation. If the jumper

    has to be there for the system to work then it MUST appear in the

    schematic. This includes the case where a ground track needs to be taken

    from a particular point, such as a star-earth design. If you're doing

    star earthing, you MUST show that on the schematic, and Eagle needs to

    know the two (or more) sides of the star are different nets.

     

    If there are 0R jumpers, they must be there for a reason. I cannot think

    of any possible reason to employ one that doesn't imply some

    significance that really MUST be shown on the schematic. If you don't

    need to show it on the schematic then you don't really need it there,

    and a better board layout is the answer you actually want.

     

    So that leaves only the possibility that you are hand-making a PCB and

    don't want to go to double-sided (or from 2-layer to 4-layer), and

    therefore intend to fit a few short wires to make up the missing bits of

    track. In that case, I would suggest that your best bet is to design a

    double-sided (or 4-layer) board with as little as physically possible on

    the extra layers, then ignore those layers when making the PCB. The

    layers that are not physically implemented on the PCB then show where

    the wire links need to be added.

     

    >Is it more expensive to move up from a 2 layer to 4 layer board or just

    >add 10 0R jumpers? Looking at real circuit boards from disk drives and

    >the like, I see many examples of 2 layer + jumper construction...

     

    I've not often seen a professionally built high-density board that used

    0R0s purely to avoid extra layers. I've seen lots where there were 0R0s

    liberally scattered for build option selection reasons (disk drives

    often do that) so that one PCB can be built for several different

    products (e.g. different drive capacities, different motor types). I

    have seen a few audio amplifiers where the PCB is single-sided and

    various signals are carried on heavy gauge bus bars instead of tracks; I

    don't know what the schematics for them look like.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of this | Windows NT crashed.

    message are purely   | I am the Blue Screen of Death.

    my opinion. Don't    | No one hears your screams.

    believe a word.      |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On Thu, 10 Jun 2010, Gary Gofstein wrote to us saying :

    >But what if the board has a significant jumper layer and there are many

    >0R jumpers that are just part of the circuitry, not selecting anything.

    >Why would I want to see these on the schematic? How does EAGLE know

    >that the net name should be the same on both sides of the jumper?

     

    Ask yourself why the jumpers are there. Remember, the schematic is the

    master definition, the board is merely an implementation. If the jumper

    has to be there for the system to work then it MUST appear in the

    schematic. This includes the case where a ground track needs to be taken

    from a particular point, such as a star-earth design. If you're doing

    star earthing, you MUST show that on the schematic, and Eagle needs to

    know the two (or more) sides of the star are different nets.

     

    If there are 0R jumpers, they must be there for a reason. I cannot think

    of any possible reason to employ one that doesn't imply some

    significance that really MUST be shown on the schematic. If you don't

    need to show it on the schematic then you don't really need it there,

    and a better board layout is the answer you actually want.

     

    So that leaves only the possibility that you are hand-making a PCB and

    don't want to go to double-sided (or from 2-layer to 4-layer), and

    therefore intend to fit a few short wires to make up the missing bits of

    track. In that case, I would suggest that your best bet is to design a

    double-sided (or 4-layer) board with as little as physically possible on

    the extra layers, then ignore those layers when making the PCB. The

    layers that are not physically implemented on the PCB then show where

    the wire links need to be added.

     

    >Is it more expensive to move up from a 2 layer to 4 layer board or just

    >add 10 0R jumpers? Looking at real circuit boards from disk drives and

    >the like, I see many examples of 2 layer + jumper construction...

     

    I've not often seen a professionally built high-density board that used

    0R0s purely to avoid extra layers. I've seen lots where there were 0R0s

    liberally scattered for build option selection reasons (disk drives

    often do that) so that one PCB can be built for several different

    products (e.g. different drive capacities, different motor types). I

    have seen a few audio amplifiers where the PCB is single-sided and

    various signals are carried on heavy gauge bus bars instead of tracks; I

    don't know what the schematics for them look like.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of this | Windows NT crashed.

    message are purely   | I am the Blue Screen of Death.

    my opinion. Don't    | No one hears your screams.

    believe a word.      |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 6/11/2010 9:43 AM, Robert Pearce wrote:

    >

    Ask yourself why the jumpers are there.

     

    They're there because a 4 layer board is more expensive than a 2 layer

    board with jumpers.

     

    track. In that case, I would suggest that your best bet is to design a

    double-sided (or 4-layer) board with as little as physically possible on

    the extra layers, then ignore those layers when making the PCB. The

    layers that are not physically implemented on the PCB then show where

    the wire links need to be added.

     

    That works for wire links, but they must be cut and stripped and

    probably installed by hand, does not work for 0R0 jumpers.

    >

    I've not often seen a professionally built high-density board that used

    0R0s purely to avoid extra layers.

     

    Maybe because the EDA tools like EAGLE don't handle it very gracefully.

     

    I've seen lots where there were 0R0s

    liberally scattered for build option selection reasons (disk drives

    often do that) so that one PCB can be built for several different

    products (e.g. different drive capacities, different motor types). I

     

    These were clearly a jumper layer. If it results in a more reliable (2

    layer), more manufacturable, lower cost board and is electrically

    equivalent - why wouldn't someone use them?

     

    If it sounds like I'm preaching, I'm not; but I have asked this question

    many times and I have never gotten a satisfactory answer. Is there

    something wrong with using a jumper layer that I don't know about? Or is

    it just that it is too time consuming or impossible to make one on most

    EDA tools?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 6/11/2010 3:22 PM, Gary Gofstein wrote:

    On 6/11/2010 9:43 AM, Robert Pearce wrote:

    >>

    >> Ask yourself why the jumpers are there.

    >

    They're there because a 4 layer board is more expensive than a 2 layer

    board with jumpers.

    >

    >> track. In that case, I would suggest that your best bet is to design a

    >> double-sided (or 4-layer) board with as little as physically possible on

    >> the extra layers, then ignore those layers when making the PCB. The

    >> layers that are not physically implemented on the PCB then show where

    >> the wire links need to be added.

    >

    That works for wire links, but they must be cut and stripped and

    probably installed by hand, does not work for 0R0 jumpers.

    >>

    >> I've not often seen a professionally built high-density board that used

    >> 0R0s purely to avoid extra layers.

    >

    Maybe because the EDA tools like EAGLE don't handle it very gracefully.

    >

    I've seen lots where there were 0R0s

    >> liberally scattered for build option selection reasons (disk drives

    >> often do that) so that one PCB can be built for several different

    >> products (e.g. different drive capacities, different motor types). I

    >

    These were clearly a jumper layer. If it results in a more reliable (2

    layer), more manufacturable, lower cost board and is electrically

    equivalent - why wouldn't someone use them?

    >

    If it sounds like I'm preaching, I'm not; but I have asked this question

    many times and I have never gotten a satisfactory answer. Is there

    something wrong with using a jumper layer that I don't know about? Or is

    it just that it is too time consuming or impossible to make one on most

    EDA tools?

     

    From reading this thread I think the main problem is we don't actually

    understand what you are trying to achieve with these jumpers.

     

    I have seen 0R SMT jumpers used on a few prototypes and they where used

    for this reason:

    The company has in house board manufacturing but only for 2-4layers and

    during development the board was too complex for a 4layer routing and

    they used SMT jumpers that looked like resistors but where just wire

    bridges in a standard SMT package. They where not on the schematic as

    the guy who routed the board just added them to get those last few

    airwires routed. This worked but if I saw a commercial product with that

    I would stay away as they where obviously cutting corners or cheap.

     

    The second reason to use 0R jumpers is the acceptable reason. If you

    look on things like hard drive logic boards, digital oscilloscopes, or

    mp3 players that have a 2/4/8 gig option to buy they use 0R jumpers to

    specify which model the device is. For example I had a sandisk mp3

    player years ago with 2GB memory and if you replace it with a 4GB chip

    the player still only uses 2GB. After you clear and set some bridges it

    work with the full 4gb. We do that as most boards are not programmed

    after full assembly and its easier to have one firmware and use 0R

    jumpers to select features in the last phase of mfg.

     

    Don't know if that's what you where talking about or now but if you try

    and word your question with a specific example where the sch has no

    jumpers and the pcb does we can find out why.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    I've just come up against this problem recently.

     

    I'm using single sided & 1206.

     

    I wanted to have something that would 'bridge' over another track (to save

    using a bit of wire), so I just used a 0R 1206 resistor - I slighly

    modified the package 'gap' between pads (on account I needed more space

    since I want to run a fine track in  between the the resistor pads.

     

    Once I created the the new library part, I simply added it to the schematic

    at more or less the same point where I wanted to be on my board file.

     

    It all works well,

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/3/2010 12:44 PM, uMinded wrote:

     

    I have seen 0R SMT jumpers used on a few prototypes and they where used

    for this reason:

    The company has in house board manufacturing but only for 2-4layers and

    during development the board was too complex for a 4layer routing and

    they used SMT jumpers that looked like resistors but where just wire

    bridges in a standard SMT package. They where not on the schematic as

    the guy who routed the board just added them to get those last few

    airwires routed. This worked but if I saw a commercial product with that

    I would stay away as they where obviously cutting corners or cheap.

    >

    They are "obviously" cutting corners? I thought 2 layer boards are much

    more reliable than 4 layer boards. What is wrong with wanting to save

    their customers' money, is that being "cheap"? Once again, no logical

    objective reason that I can see...

     

    If an SMT resistor is reliable, why would an SMT jumper be less

    reliable? If you could somehow tell that there were a few extra

    resistors on a board, would you declare it to be cheap or cutting corners?

     

    I suspect the real reason this is not done more often is simply that CAD

    tools don't handle it gracefully. But if someone does have an answer to

    why it is a bad idea, I'd like to hear it...

     

    The second reason to use 0R jumpers is the acceptable reason. If you

    What makes them "acceptable" in this context but not in a jumper layer

    context?

     

    By the way, the disk drive in question was from the top rated

    manufacturer and was produced in the early 2000's. In my experience,

    volume commodity manufacturers favor double or single (yes!) layer

    boards wherever possible.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 2010-06-12 00:22:30 +0200, Gary Gofstein <nospam@use.forum.net> said:

     

    If it sounds like I'm preaching, I'm not; but I have asked this

    question many times and I have never gotten a satisfactory answer. Is

    there something wrong with using a jumper layer that I don't know

    about? Or is it just that it is too time consuming or impossible to

    make one on most EDA tools?

     

    There are several ways to handle jumpers, I use two of them. I etch the

    first edition of most boards myself.

     

     

    1) I route long jumpers on the top layer and use bare wires. Make the

    tracks going to the via as fat as possible, preferably the same

    diameter as the via, so the eyelet will stay on the board when you

    drill.

     

    2) short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic. See attach. Yes, I

    ignore the airwaire on the board.  These 1206 jumpers are used mostly

    for connecting GND planes, i.e. different parts of the same polygon.

     

    Soldering an 1206 0R resistor is a lot less work than drilling two

    holes and wiggling a wire through them. For boardhouse made boards, 2

    layers is enough for me.

     

    Yes, it would be nice if Eagle could see the jumper as part of the net,

    but this would involve different treatments of components that are part

    of the net and components that are not. A different layer would not

    solve that.

     

     

    --

    Eur van Andel  eur@fiwihex.nl

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Eur van Andel wrote on Mon, 12 July 2010 08:10

    short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic.

     

    SMD resistors used in this role should not be on the schematic, since they

    are a artifact of routing, and do not relate to the circuit itself.

     

    Currently there is no way to do this in Eagle, but that would be a nice

    idea.

     

    Quote:

    Yes, it would be nice if Eagle could see the jumper as part of the net,

     

    but this would involve different treatments of components that are part

     

    of the net and components that are not.

     

    I think if this were added it would have to be in the ROUTE command where

    it understands special packages you define as jumpers.  You should be able

    to place them anywhere in a route, just like vias.  There would need to be

    a list of allowable jumpers per net class so that the auto router knows

    what it can do.  Each type of jumper would also need its own cost in the

    auto router.

     

    Note that these jumpers must not show up in the schematic.  You must be

    free to add them or rip them up without having to edit the schematic.  They

    do need to be in the board data so that BOM tools can find them.

     

    While all this is nice, it sounds like it would be considerable effort to

    add to Eagle.  If I got to pick I'd rather CadSoft work on more flexible

    package definition so that you can suppress some DRC errors from deliberate

    overlaps within a package, and allow for multiple symbols per device (gate)

    with possibly different numbers of pins.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/12/2010 5:10 AM, Eur van Andel wrote:

    On 2010-06-12 00:22:30 +0200, Gary Gofstein <nospam@use.forum.net> said:

    >

    >> If it sounds like I'm preaching, I'm not; but I have asked this

    >> question many times and I have never gotten a satisfactory answer. Is

    >> there something wrong with using a jumper layer that I don't know

    >> about? Or is it just that it is too time consuming or impossible to

    >> make one on most EDA tools?

    >

    There are several ways to handle jumpers, I use two of them. I etch the

    first edition of most boards myself.

    >

    >

    1) I route long jumpers on the top layer and use bare wires. Make the

    tracks going to the via as fat as possible, preferably the same diameter

    as the via, so the eyelet will stay on the board when you drill.

    >

    2) short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    need to be in the BOM, so also in the schematic. See attach. Yes, I

    ignore the airwaire on the board. These 1206 jumpers are used mostly for

    connecting GND planes, i.e. different parts of the same polygon.

    >

    Soldering an 1206 0R resistor is a lot less work than drilling two holes

    and wiggling a wire through them. For boardhouse made boards, 2 layers

    is enough for me.

    >

    Yes, it would be nice if Eagle could see the jumper as part of the net,

    but this would involve different treatments of components that are part

    of the net and components that are not. A different layer would not

    solve that.

    >

    >

    I have heard that some CAD packages have a designated jumper layer that

    they can route on. The rules for this layer are derived from the type of

    jumper that are allowed to be generated ( fixed length wire, 0R thru

    hole resistor, 0R SMD resistors ). This allows the CAD software to keep

    track of the net connections ( through the special layer) and keep these

    jumpers off the schematic. It is not just another copper layer, EAGLE

    already has plenty of those. The special layer is not ever output, just

    used to contain the routes that belong to the jumper components.

     

    There are a lot of ways to make the software handle a "jumper layer"

    functionality...I was just pointing this out as an example.

     

    The reason for bringing up the topic in this thread is not related to

    how work around the problem in EAGLE, but rather to a poster's assertion

    that the jumpers /must/ appear in the schematic. I believe the original

    poster was talking about "jumper layer" jumpers rather than "option

    selecting" jumpers and that these kind of jumpers are not needed or

    desired in the schematic, only the BOM.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On 7/12/2010 6:15 AM, Olin Lathrop wrote:

    Eur van Andel wrote on Mon, 12 July 2010 08:10

    >> short jumpers are done with 0R reistors, 1206 foorprint. Yes, these

    >> need to be in the BOM, so also in the schematic.

    >

    SMD resistors used in this role should not be on the schematic, since they

    are a artifact of routing, and do not relate to the circuit itself.

    >

    Currently there is no way to do this in Eagle, but that would be a nice

    idea.

    >

    Quote:

    >> Yes, it would be nice if Eagle could see the jumper as part of the net,

    >>

    >> but this would involve different treatments of components that are part

    >>

    >> of the net and components that are not.

    >

    I think if this were added it would have to be in the ROUTE command where

    it understands special packages you define as jumpers. You should be able

    to place them anywhere in a route, just like vias. There would need to be

    a list of allowable jumpers per net class so that the auto router knows

    what it can do. Each type of jumper would also need its own cost in the

    auto router.

    >

    Note that these jumpers must not show up in the schematic. You must be

    free to add them or rip them up without having to edit the schematic. They

    do need to be in the board data so that BOM tools can find them.

    >

    While all this is nice, it sounds like it would be considerable effort to

    add to Eagle. If I got to pick I'd rather CadSoft work on more flexible

    package definition so that you can suppress some DRC errors from deliberate

    overlaps within a package, and allow for multiple symbols per device (gate)

    with possibly different numbers of pins.

    >

    This is also an excellent way to do it. The advantage of the dedicated

    layer approach is that it only requires relaxation of some of EAGLE's

    rules to implement the functionality, rather than new functionality.

     

    In this way it is analogous to the examples you've given where EAGLE's

    insistence on 1:1 correspondance and enforcing rules that are meant to

    keep newbies out of trouble are becoming a problem. A warning is more

    appropriate than a prohibition in these cases...