to: Eagle forum
re: How is default VIA drill size set?
Tue 6/15/2010 4:52 pm
The default VIA drill size appears to be drill #2 in "options" menu, "set",
"drill" tab, .023622 (apparently a rounded .6 mm). Which, sadly, is
smaller than the default DRC "sizes" tab, "minimum drill". (Changing the
option in the "drill tab" doesn't seem to change the VIA drill size.)
Where in Eagle is the default VIA drill size set?
======================================
j.g. owen * email: mailto:owen_bda4@yahoo.com
web: http://owenlabs.org
======================================
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.