EAGLE User Support (English) SMD pad sizes in rcl.lib (Kemet vs non)
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
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 1462 views
  • Users 0 members are here
Related

SMD pad sizes in rcl.lib (Kemet vs non)

Former Member
Former Member over 15 years ago

Other than the obvious size difference, what is the functional difference

between the Kemet packages and the non-kemet in the rcl.lib.  Specifically,

I'm looking at the 0402 and the 0402K for capacitors and resistors.  When

would I use one vs the other?  Why are there two different packages for

0402?  Any insight into the library package design and usage would be

greatly appreciated.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 15 years ago

    On Tue, 28 Sep 2010, Robert Palmer wrote to us saying :

    >Other than the obvious size difference, what is the functional difference

    >between the Kemet packages and the non-kemet in the rcl.lib.  Specifically,

    >I'm looking at the 0402 and the 0402K for capacitors and resistors.  When

    >would I use one vs the other?  Why are there two different packages for

    >0402?

     

    The 0402 refers to the size of the actual component. This size is

    standard, and all 0402 parts are the same size. However, this is not the

    same as the size of the PCB footprint because the pads have to be large

    enough to allow the ends of the component to be soldered. Component

    manufacturers recommend a PCB footprint to use, which is sometimes

    different depending on whether you will be using wave or reflow

    soldering. As it happens, most manufacturers recommend the same pad size

    and spacing for their 0402 capacitors. For some reason Kemet recommend a

    different one.

     

    The best thing is to check the data sheet for the actual components

    you're using and see whether it recommends the Kemet pads or the more

    common ones. If they're free issued by your board house (as my preferred

    board house do for common resistors and ceramic caps) then check with

    them as to which footprint they prefer.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | Pickle's Law:

    this message are    |   If Congress must do a painful thing,

    purely my opinion.  |   the thing must be done in an odd-number year.

    Don't believe a     |

    word.               |