Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) C-header generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 184 subscribers
  • Views 320 views
  • Users 0 members are here
Related

C-header generator

Former Member
Former Member over 15 years ago

I think a tool (or a script, TBD) able to read .sch file and generate .c/.h file with #define will spare a lot of time.

 

I mean something able to outputs something like (in case of a PIC):

 

#define PORTAbits.RA3 LED

 

If UC pin will have an option "input / output / open drain / pull-up enabled / analog", the generator will also be able to generate mask for ports direction regs:

 

#define TRISA_MASK 0x1234

 

The shematic errors checker will be able to generate new type of errors :

- "UC1.RA4 and UC2.RB6 connected together and defined as output"

- "UC1.RB14 defined as input and unconnected. Don't leave unused inputs unconnected"

 

A such powerful tool could spare a lot of time and avoid a lot of errors!

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 15 years ago

    Matt Collinge wrote on Mon, 19 July 2010 08:50

    I think a tool (or a script, TBD) able to read .sch file and generate

    .c/.h file with #define will spare a lot of time.

     

    I mean something able to outputs something like (in case of a PIC):

     

    #define PORTAbits.RA3 LED

     

    I have something like that in my PIC http://www.embedinc.com/pic but it

    doesn't interface with Eagle.  Check out the

    http://www.embedinc.com/pic/prepic.txt.htm commands /INBIT and /OUTBIT.

    These allow you to define a symbolic name for each I/O line and how it is

    used.

     

    I hadn't thought of merging this with Eagle schematics, but that's a good

    idea.  I'm not sure which direction it should work in though.  If starting

    with Eagle, the net name connected to a pin can become the pin name in the

    PIC source code, but it won't know the pin direction.  It will be tricky to

    automate this, but it could be possible.  Going the other direction may

    make more sense in that the source code should probably be the master

    definition and the schematic should reflect it.  However, I don't think pin

    directions can be changed on the fly for a instance of a part in the

    schematic.  Actually this is a problem with both methods.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    I think it should be the schematic which would define the pin names.  The schematic pins should be annotated with pin directions, maybe from the IC library.  They can be in, out, i/o, or special/alternate function.  This would allow the header generator to define either specific pin names for each, or a generic name which supports all directions and special or alternate functions.

    • Cancel
    • Vote Up 0 Vote Down