EAGLE User Support (English) Break away rails?
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 773 views
  • Users 0 members are here
Related

Break away rails?

Former Member
Former Member over 15 years ago

Could someone provide some tips on how to add "break away rails" to a

PCB?  Is there anything in the Eagle documentation/tutorials that offer

any insight.  I know what they are and have had break away rails added

to may boards that I have worked on, but I have not done this part of

the layout.  The PCB houses call the tabs with holes which attach to the

main board "mouse bites".  This is just done with drilled holes I

assume, but I have no idea of what size drill or how closely to space

them.  If anyone has an example of this in Eagle that they'd be willing

to share I'd be most grateful.

 

Regards,

 

Michael

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 15 years ago

    Michael Sansom wrote:

    Could someone provide some tips on how to add "break away rails" to a

    PCB?

     

    The board house noramlly wants to add thoose themselves.

     

    Just tell them if there are places you do not want them.

    There are many variants.

    For example they can be made a bit into the board so when they break

    ther eis nothing stickin out past the drawn outer line, bu tin that case

    make room for that construction (leave space close to the border there)

    after discussing with manufacturer.

     

    Or maybe simple bridges in the corners are an option for small boards,

    easy to cut manually.

     

    Bottom line: first ask manufacturer.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago

    Michael Sansom wrote:

    Could someone provide some tips on how to add "break away rails" to a

    PCB?

     

    The board house noramlly wants to add thoose themselves.

     

    Just tell them if there are places you do not want them.

    There are many variants.

    For example they can be made a bit into the board so when they break

    ther eis nothing stickin out past the drawn outer line, bu tin that case

    make room for that construction (leave space close to the border there)

    after discussing with manufacturer.

     

    Or maybe simple bridges in the corners are an option for small boards,

    easy to cut manually.

     

    Bottom line: first ask manufacturer.