EAGLE User Support (English) Don't understand EagleCAD's cryptic "Width" error on my new part
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
  • Replies 8 replies
  • Subscribers 179 subscribers
  • Views 2540 views
  • Users 0 members are here
Related

Don't understand EagleCAD's cryptic "Width" error on my new part

Former Member
Former Member over 15 years ago

Hi,

 

I created a new part and use it on my *.brd.  I run a check an EagleCAD

reports "Width" with not much explanation.  Please see the attached

image.  Thanks for any tips.

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 15 years ago

    Am 07.08.2010 01:47, schrieb AL:

    Hi,

     

    I created a new part and use it on my *.brd.  I run a check an EagleCAD

    reports "Width" with not much explanation.  Please see the attached

    image.  Thanks for any tips.

     

    Obviously the SMD pads are smaller than the minimum width value for copper

    objects defined in the Design Rules' Sizes tab.

     

    By the way: All the error messages are described in the manual, in the DRC

    chapter. Example:

     

    Width:

    Minimum width violation of a copper object. Defined by Minimum Width in

    the Design Rules (Sizes tab) or, if defined, by the track parameter Width of

    a referring net class. The higher one of the given values will be taken for

    this check.

    Also the line width of vector font texts in signal layers will be checked.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Richard_H

    Also the line width of vector font texts in signal layers will be checked.

     

    How do we determine the 'Width' of a vector font texts in signal layers?

     

    The Properties box of a Text object has no reference to the Width but to the

    Ratio.

     

    The Help says

    >>The height of characters and the line width can be changed with the CHANGE

    >>commands:

    CHANGE SIZE text_size ...

    CHANGE RATIO ratio ...

    Maximum text height: 2 inches

    Maximum line width: 0.51602 inch (13.1 mm)

    Ratio: 0...31 (% of text height).

    <<

     

    The Properties box of a Text object does not refer to the Text Height

    either, so the only way to get rid of the 'Width' warning in the Drc is to

    gradually increase the Ratio of the Vector font until the warning goes. 24%

    in the sample I've enclosed.This gives a very 'Clunky' text and so I use a

    proportional font and turn off the warnings.

     

    Tony Hunt

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 15 years ago in reply to Richard_H

    Also the line width of vector font texts in signal layers will be checked.

     

    How do we determine the 'Width' of a vector font texts in signal layers?

     

    The Properties box of a Text object has no reference to the Width but to the

    Ratio.

     

    The Help says

    >>The height of characters and the line width can be changed with the CHANGE

    >>commands:

    CHANGE SIZE text_size ...

    CHANGE RATIO ratio ...

    Maximum text height: 2 inches

    Maximum line width: 0.51602 inch (13.1 mm)

    Ratio: 0...31 (% of text height).

    <<

     

    The Properties box of a Text object does not refer to the Text Height

    either, so the only way to get rid of the 'Width' warning in the Drc is to

    gradually increase the Ratio of the Vector font until the warning goes. 24%

    in the sample I've enclosed.This gives a very 'Clunky' text and so I use a

    proportional font and turn off the warnings.

     

    Tony Hunt

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Tony Hunt schrieb:

     

    >> Also the line width of vector font texts in signal layers will be checked.

     

    How do we determine the 'Width' of a vector font texts in signal layers?

     

    The Properties box of a Text object has no reference to the Width but to the

    Ratio.

     

    ...and the height (size). So, you can easily determine the "width" of a

    text by multiplying size and ratio.

     

    The Properties box of a Text object does not refer to the Text Height

    either,

     

    --> "size"

     

    so the only way to get rid of the 'Width' warning in the Drc is to

    gradually increase the Ratio of the Vector font until the warning goes.

     

    Or:

    - increase the height/size of the text;

    - decrease your minimum width in DRC.

     

    You don't need to do any of these gradually since you can easily

    calculate the relations, see above.

     

    24% in the sample I've enclosed.This gives a very 'Clunky' text

     

    Indeed, ratio 24% is not very fine looking - obviously, your text is too

    small for the required minimum width.

     

    and so I use a proportional font and turn off the warnings.

     

    ...which is processed as vector font when you produce gerber files, so

    your board will have the "clunky" text.

     

    You need to decide what your minimum width is, related to your board

    house limitations (or pricing), and set up your DRC accordingly. Then,

    if you want text objects to also comply with these parameters, you

    really need to modify size and/or ratio until DRC does not complain. For

    plain readability of text on a board, it maybe OK to fall below those

    limits, however - talk to your board house.

     

    Tilmann