Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) LTSpice no more supported?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 927 views
  • Users 0 members are here
Related

LTSpice no more supported?

e14 Contributor
e14 Contributor over 10 years ago

Hello:

with version7.5, I noticed that there is no toolbar for LTSpice, is-it no more supported?

 

thank you

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to autodeskguest

    Hi Warren.

     

    Is there another way to integrate Eagle 7.5 with LTSpice IV on Linux?

     

    I'm running LTSpice with Wine (Windows emulator) and its running pretty well.

     

    Thanks in advance.

     

    --

    Fernando F.

    http://desconstruindo.eng.br

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to autodeskguest

    Works fine, thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    On 10/01/2016 9:13 a.m., Jacques MARTIN wrote:

    thanks for reply

     

     

    Also I noticed that's impossible to display the "command text" buttons

    (which I'm using) and the LT and PCBsim toolbar in the same time

    am I wrong?

     

     

    The LT and PCBsim toolbar and the "command text" menu/buttons are one

    and the same thing.  You cannot split them into two areas of the display.

     

    Put another way, the toolbar, as you call it, is simply the command text

    menu showing images instead of words.

      See the HELP > Editor Commands > Menu

     

     

    You need to set up a menu command that includes all of what you need.

    LTSpice,PCBSim and your command text menu items and then position the

    resulting toolbar/menu where you desire

     

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    thanks for reply

    I re-installed the software and now it's OK

    Mysteriously the lines

    MENU \

       '[LTspice.png] LT Spice simulation {\

                        Export: RUN ltspice.ulp /E; |\

                        Export Setup: RUN ltspice.ulp /E /S; |\

                        Export Group: RUN ltspice.ulp /E /G; |\

                        Import: RUN ltspice.ulp /I; \

    has disappeared from eagle.scr, may be during installing felicitas pcbsim? I don't know

     

    Also I noticed that's impossible to display the "command text" buttons (which I'm using) and the LT and PCBsim toolbar in the same time

    am I wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 10/01/2016 7:58 a.m., warrenbrayshaw wrote:

    On 9/01/2016 10:26 p.m., Jacques MARTIN wrote:

    Hello:

    with version7.5, I noticed that there is no toolbar for LTSpice, is-it

    no more supported?

     

    thank you

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/171067

     

     

    The LTSpice button only shows up in the schematic editor.

    It is still there in version 7.5

     

    HTH

    Warren

     

     

    I should clarify, this is for Windows only.

    The LTSpice ULP has to date only been supported on Windows.

     

    On MAC and Linux the LTSpice button is not presented.

    i.e. it is not included in the eagle.scr

     

    Maybe in earlier eagle versions it was presented for the MAC as it was

    envisaged that it would become available. I don't know if this is the case.

     

    WArren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    On 9/01/2016 10:26 p.m., Jacques MARTIN wrote:

    Hello:

    with version7.5, I noticed that there is no toolbar for LTSpice, is-it

    no more supported?

     

    thank you

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/171067

     

     

    The LTSpice button only shows up in the schematic editor.

    It is still there in version 7.5

     

    HTH

    Warren