Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Bug in 7.3, can't export to TIF file
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 188 subscribers
  • Views 2983 views
  • Users 0 members are here
Related

Bug in 7.3, can't export to TIF file

autodeskguest
autodeskguest over 11 years ago

In version 7.3 on Windows 7 64 bit, there seems to be a bug in exporting a

board to a TIF image file.  In the board editor, if I run "EXPORT IMAGE

\temp\a.tif" I always get a popup that says "Out of memory while writing

'/temp/a.tif'".  This happens regardless of resolution.  For example,

"EXPORT IMAGE \temp\a.tif 50" fails the same way, even though that would

have only required 320 x 552 pixels in my case.

 

This is a important feature to me since that's how I make assembly

drawings.  The same procedure to make the same assembly drawing worked fine

in version 5.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    I just installed latest Eagle for 64-bit Linux with the Element 14 free trial key on an Xubuntu 14.04 LTS x64 stable system.  When I try to export the Arduino project to ANY graphics format, I get the same result i.e. "Out of memory while writing ...".  So, this is not just Windows.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    I just installed latest Eagle for 64-bit Linux with the Element 14 free trial key on an Xubuntu 14.04 LTS x64 stable system.  When I try to export the Arduino project to ANY graphics format, I get the same result i.e. "Out of memory while writing ...".  So, this is not just Windows.