Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Re: Need a Way to Get Rid of CAM .GPI Files
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 191 subscribers
  • Views 2358 views
  • Users 0 members are here
Related

Re: Need a Way to Get Rid of CAM .GPI Files

e14 Contributor
e14 Contributor over 15 years ago

On 1/18/2011 1:48 PM, James Morrison wrote:

I know this has come up before but I'm having to delete a lot of these

lately and it is annoying.

 

I have no use for the .gpi files that are generated when creating

gerbers. We need a way to add a tab to the CAM file (last one I would

think) that

can specify a system command to run. Then users could do all kinds of

things for production file generation, including running a command line to

remove those silly .gpi files.

 

I can't count how many thousands of those files I have deleted--that is all

wasted time that I'll never get back. And I don't want to have to go to a

command line to do it manually--the tool should allow a way to clean up

automatically.

 

James.

thought I was the only one...why not just make their generation

optional? or get rid of it? I don't find them useful, does anyone?

 

  • Sign in to reply
  • Cancel
Parents
  • hbridge99
    hbridge99 over 8 years ago

    Still undone 02/2018?

     

    How hard is it to suppress the output of file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hbridge99
    hbridge99 over 8 years ago

    Still undone 02/2018?

     

    How hard is it to suppress the output of file?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rachaelp
    rachaelp over 8 years ago in reply to hbridge99

    hbridge99  wrote:

     

    Still undone 02/2018?

     

    How hard is it to suppress the output of file?

     

    There is a completely new CAM in 8.6.0, I've just checked explicitly for this file but it is not being generated by the new CAM. There is a .gbrjob file exported now but in the main Gerber section you can uncheck a box to turn that off. The output now simply contains the specified Gerber and Excellon files, nothing else.

     

    Best Regards,


    Rachael