EAGLE User Support (English) Using Eagle on two systems, with library on USB stick
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
  • Replies 8 replies
  • Subscribers 180 subscribers
  • Views 2160 views
  • Users 0 members are here
Related

Using Eagle on two systems, with library on USB stick

Former Member
Former Member over 14 years ago

I use EAGLE on a desktop and a laptop for the same projects. A complication

happens when I edit a library part and I want the project on both systems to

update from the same library. The part in a project is linked to a library

at a certain path. If I copy the library to a USB stick and try to update

the library part in a project to the laptop, the EAGLE on the laptop doesn't

know to update from the library on the USB stick. It only updates from the

library in the original path.

 

Do I need to have libraries in exactly the same path names, and same drive

letters common to both systems to make a part update from the library it is

originally from? Is there a way to point it to "mylibrary.lib" on the USB

stick and update the part in the board and schematic?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • crlMidi
    crlMidi over 11 years ago

    It seems appropriate to reactivate this old thread because it explains the situation well, and there don't seem to be any more recent contributions.

     

    I'm introducing some beginners to Arduino and expect to use Eagle to document the circuitry. Drawing schematics isn't too difficult; Sparkfun and Adafruit have provided nice libraries, and Dave Young has supplied a complete set of Arduinos as devices. We won't often be making PCBs.

     

    A major advantage of Eagle is that it runs on both  Windows and Linux; not everybody can replace their XP machines lubuntu is a good choice for saving all but the oldest. I'ts also a good way of getting beginners to use Linux from the start. TinyCAD is brilliant for amateurs, but it wants users to write files in the protected Program Files area and can't be ported to Linux.

     

    Like other contributors here, my friends will be working on more than one PC (at home & and in my house), and I'd like to know what's the current situation or "least worst" workaround with Eagle. The basic problem is that both Linux and Windows, as well as many applications, still force users to use their own user areas. This may be good for security, but it's totally stupid, even for sharing photos among family members.

     

    Perhaps a workaround with Eagle might be to use a shared directory on each PC for working, and to get a backup application like Create Synchronicity to sychronise this with the Dropbox, Ubuntu One, etc. directories in a user space. I tried something like that but got into a bit of a mess, with multiple copies of libraries and so on.

     

    So, my question is: has anyone now found a reliable way of sharing projects and libraries tidily, without any special programming? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to crlMidi

    On 3/20/2014 10:57 AM, Christopher Lee wrote:

    Perhaps a workaround with Eagle might be to use a shared directory on

    each PC for working, and to get a backup application like Create

    Synchronicity to sychronise this with the Dropbox, Ubuntu One, etc.

    directories in a user space. I tried something like that but got into a

    bit of a mess, with multiple copies of libraries and so on.

     

    Hi Christopher,

     

    I hope you're doing well. If you're going to have multiple collaborators

    working on the same project then the standard solution is to use some

    sort of Version control system.

     

    A popular setup is to use something like GitHub to store all of the

    design files. Users can then checkout the files and modify them, when

    they're done they can then push the changes back to github. Usually

    there will be an administrator who can control what changes make it back

    to the main set of files.

     

    This is a very high-level description and there are lots of variations

    on the theme. For example Ubuntu has version control system called

    Bazaar that interfaces with Launchpad their GitHub clone.

     

    Others will chime in with suggestions.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to crlMidi

    On 3/20/2014 10:57 AM, Christopher Lee wrote:

    Perhaps a workaround with Eagle might be to use a shared directory on

    each PC for working, and to get a backup application like Create

    Synchronicity to sychronise this with the Dropbox, Ubuntu One, etc.

    directories in a user space. I tried something like that but got into a

    bit of a mess, with multiple copies of libraries and so on.

     

    Hi Christopher,

     

    I hope you're doing well. If you're going to have multiple collaborators

    working on the same project then the standard solution is to use some

    sort of Version control system.

     

    A popular setup is to use something like GitHub to store all of the

    design files. Users can then checkout the files and modify them, when

    they're done they can then push the changes back to github. Usually

    there will be an administrator who can control what changes make it back

    to the main set of files.

     

    This is a very high-level description and there are lots of variations

    on the theme. For example Ubuntu has version control system called

    Bazaar that interfaces with Launchpad their GitHub clone.

     

    Others will chime in with suggestions.

     

    hth,

    Jorge Garcia