Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Missing components in the library...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 188 subscribers
  • Views 4113 views
  • Users 0 members are here
Related

Missing components in the library...

e14 Contributor
e14 Contributor over 15 years ago

Hello,

Still using the free version and still at newby silly question level.

I am creating (at least trying to) my first PCB board which is going to be a PMW. I started by ordering all the coponents from digikey (got an head acke with their web tool..)

 

My coponents are in my ordering list:

* SN74ACC14N: Found it sounds good

* EVU-F3lFL3B14 (potentiometer): even with the datacheet I do not find it

* 1N5817 (diode): can not find it... 9there is of course some close enough)

* BUL704 (NPN) was not able to find it directly but using the number of the datasheet TO-220 whihc was not in the database either I end up finding it using TO220...

* 1N914BTR (diode) was not able to find it... (same thing found stuff close enough after some time but my electronic level is limited)

 

And the list is going a like that on every conponent.

My frustration level in rising, I spent more time looking ofr the components that I will spend on creating the board (step that I have note reached yet...)

 

 

So simple questions:

1) I am doing something wrong?

2) If I am not doing anything wrong where can I find an extended library of components?

3) If netheir one or two are possible, how do you proceed on your side to order components? you try to see if they exist in Eagle then in DIgikey (for example) and then only order them?

 

Thank you for your help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 15.03.2011 21:51, schrieb badbad2142:

    Hello,

    Still using the free version and still at newby silly question level.

    I am creating (at least trying to) my first PCB board which is going to be a PMW. I started by order all the coponents for m digikey (got an head acke with their web tool..)

     

    My coponents are:

    • SN74ACC14N: Found it sounds good

    • EVU-F3lFL3B14 (potentiometer): even wiht the datacheet I do not find it

     

     

    Sorry, no email adress to send the extended lbr.

     

     

    • 1N5817 (diode): can not find it...

     

    Use diode.lbr -> device DIODE- with package variant DO41-10 and set the

    VALUE to 1N5817.

     

     

    • BUL704 (NPN) was not able to find it directly but using the number of the datasheet TO-220 whihc was not in the database either I end up finding it using TO220...

     

    Use transistor.lbr -> device *-NPN- with package variant TO220 and set

    the VALUE to BUL704.

     

    • 1N914BTR (diode) was not able to find it...

     

    Use diode.lbr -> device DIODE- with package variant DO35-10 and set the

    VALUE to 1N914BTR.

     

     

    And the list is going and going like that on every conponent.

    My frustration level in rising, I spent more time looking ofr the components that I will spend on

    > creating the board (step that I have note reached yet...)

     

    Plase read

    HELP USE (enter)

    HELP ADD (enter)

     

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thank you both for your answers.

    My mail adress is abessy@free.fr ;-)


    I was hoping to spend more time to design the PCB and less on the components selection but I understand that all of them can not exists. It is just hard from the point of view that I am not doing PCB often (in fact it is the first) nor I am working in the electronic field so I am not fluent with the components equivalence (yet).

     

    But I will get at it then...

     

    Thank you again for your answers.

    Regards

    Alexandre Bessy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    badbad2142 wrote:

    Thank you both for your answers.

    My mail adress is abessy@free.fr (mailto:abessy@free.fr) image

     

    I was hoping to spend more time to design the PCB and less on the components selection but I understand that all of them can not exists. It is just hard from the point of view that I am not doing PCB often (in fact it is the first) nor I am working in the electronic field so I am not fluent with the components equivalence (yet).

     

     

    Just a comment from a guy who does electronics design for >25 years:

    Packaging, component selection and the creation of library parts is

    boring but it is often 50% of the job. Especially on cost critical

    designs. So it is very important to learn the library editor of a new

    CAD system very soon. Eagle isn't particularly easy to learn in that

    respect but with persistence you'll get there.

     

    Afterwards, when you haven't used the program for a while it is normal

    to forget things.

     

    By the way, the Digikey search engine is hands down the best there is,

    there ever was. If you learn how to use that (easy) it becomes a

    wonderful tool to find electronic parts. And now they also let you sort

    by price.

     

     

    But I will get at it then...

     

     

    En peu du vin rouge, du fromage et la bonne musique ... and it will all

    come together nicely image

     

    --

    Cordialement, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 3/31/2011 5:49 PM, Joerg wrote:

    Gary Gofstein wrote:

    >> On 3/31/2011 8:42 AM, badbad2142 wrote:

    >>> Thank you all for your inputs. To be honest I was long to reply

    >>> because I did not realize that a third page was there.

    >>>

    >>> Paul: Yes I have two jumpers.

    >>> Gary: I hope you are right and that I will get away with it this time.

    >>> I will keep your advise in mind for my next design (cmos legs inputs

    >>> to be connected) . I will replace the capacitors by ceramic. My board

    >>> being home made (and it is the first one that I do) I am only one side

    >>> (it looks like this:

    >>> http://i203.photobucket.com/albums/aa14/badbad214/Eagle/IMG_9090.jpg

    >>> it has not been perfectly clean yet). It is also the reason why I did

    >>> not care about the text (for this time at least).

    >>> Joerg: I will try to improve with the ceramic capacitors but if it

    >>> does not do it I will have to try again...

    >>>

    >>> Thank you all again!

    >>>

    >> You don't replace the caps with ceramic, you keep them, and then add

    >> ceramic /as close to the chip as possible/ in parallel with the

    >> electrolytics. ...

    >

    Yup, that's how it's done.

     

    >

    >>            ... If you use 74AC, I doubt it will work, 74HC chips,

    >> maybe it works... never use 74AC unless you really know what you're

    >> doing. If you already made the board, I would just solder a 0.1 ceramic

    >> between pins 14 and 7 on the bottom of the board, that should do it.

    >

    On 74HC leaving inputs open usually doesn't work either. They'll waft

    around, getting into the linear range around VCC/2, something starts

    oscillating and the guy next door gets mad because his FM radio always

    quits when the circuit is running image

     

    A 74AC with open inputs is a loose cannon. Sometimes oscillation at a

    high enough frequency can cause a chip to self-destruct. Since the

    74AC14 contains Schmitt inputs it might not self-destruct if replaced

    with a 74HC14. Maybe, but I wouldn't hold my breath.

     

    100% agreement, I was trying to say that AC without close bypassing will

    go crazy for sure while HC might tolerate it. Any open inputs will cause

    erratic circuit function and I see this mistake a lot on circuits on the

    internet. Usually with comments that some builders "couldn't get it to

    work." Of course...

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 3/31/2011 5:49 PM, Joerg wrote:

    Gary Gofstein wrote:

    >> On 3/31/2011 8:42 AM, badbad2142 wrote:

    >>> Thank you all for your inputs. To be honest I was long to reply

    >>> because I did not realize that a third page was there.

    >>>

    >>> Paul: Yes I have two jumpers.

    >>> Gary: I hope you are right and that I will get away with it this time.

    >>> I will keep your advise in mind for my next design (cmos legs inputs

    >>> to be connected) . I will replace the capacitors by ceramic. My board

    >>> being home made (and it is the first one that I do) I am only one side

    >>> (it looks like this:

    >>> http://i203.photobucket.com/albums/aa14/badbad214/Eagle/IMG_9090.jpg

    >>> it has not been perfectly clean yet). It is also the reason why I did

    >>> not care about the text (for this time at least).

    >>> Joerg: I will try to improve with the ceramic capacitors but if it

    >>> does not do it I will have to try again...

    >>>

    >>> Thank you all again!

    >>>

    >> You don't replace the caps with ceramic, you keep them, and then add

    >> ceramic /as close to the chip as possible/ in parallel with the

    >> electrolytics. ...

    >

    Yup, that's how it's done.

     

    >

    >>            ... If you use 74AC, I doubt it will work, 74HC chips,

    >> maybe it works... never use 74AC unless you really know what you're

    >> doing. If you already made the board, I would just solder a 0.1 ceramic

    >> between pins 14 and 7 on the bottom of the board, that should do it.

    >

    On 74HC leaving inputs open usually doesn't work either. They'll waft

    around, getting into the linear range around VCC/2, something starts

    oscillating and the guy next door gets mad because his FM radio always

    quits when the circuit is running image

     

    A 74AC with open inputs is a loose cannon. Sometimes oscillation at a

    high enough frequency can cause a chip to self-destruct. Since the

    74AC14 contains Schmitt inputs it might not self-destruct if replaced

    with a 74HC14. Maybe, but I wouldn't hold my breath.

     

    100% agreement, I was trying to say that AC without close bypassing will

    go crazy for sure while HC might tolerate it. Any open inputs will cause

    erratic circuit function and I see this mistake a lot on circuits on the

    internet. Usually with comments that some builders "couldn't get it to

    work." Of course...