Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Missing components in the library...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 188 subscribers
  • Views 4120 views
  • Users 0 members are here
Related

Missing components in the library...

e14 Contributor
e14 Contributor over 15 years ago

Hello,

Still using the free version and still at newby silly question level.

I am creating (at least trying to) my first PCB board which is going to be a PMW. I started by ordering all the coponents from digikey (got an head acke with their web tool..)

 

My coponents are in my ordering list:

* SN74ACC14N: Found it sounds good

* EVU-F3lFL3B14 (potentiometer): even with the datacheet I do not find it

* 1N5817 (diode): can not find it... 9there is of course some close enough)

* BUL704 (NPN) was not able to find it directly but using the number of the datasheet TO-220 whihc was not in the database either I end up finding it using TO220...

* 1N914BTR (diode) was not able to find it... (same thing found stuff close enough after some time but my electronic level is limited)

 

And the list is going a like that on every conponent.

My frustration level in rising, I spent more time looking ofr the components that I will spend on creating the board (step that I have note reached yet...)

 

 

So simple questions:

1) I am doing something wrong?

2) If I am not doing anything wrong where can I find an extended library of components?

3) If netheir one or two are possible, how do you proceed on your side to order components? you try to see if they exist in Eagle then in DIgikey (for example) and then only order them?

 

Thank you for your help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 15.03.2011 21:51, schrieb badbad2142:

    Hello,

    Still using the free version and still at newby silly question level.

    I am creating (at least trying to) my first PCB board which is going to be a PMW. I started by order all the coponents for m digikey (got an head acke with their web tool..)

     

    My coponents are:

    • SN74ACC14N: Found it sounds good

    • EVU-F3lFL3B14 (potentiometer): even wiht the datacheet I do not find it

     

     

    Sorry, no email adress to send the extended lbr.

     

     

    • 1N5817 (diode): can not find it...

     

    Use diode.lbr -> device DIODE- with package variant DO41-10 and set the

    VALUE to 1N5817.

     

     

    • BUL704 (NPN) was not able to find it directly but using the number of the datasheet TO-220 whihc was not in the database either I end up finding it using TO220...

     

    Use transistor.lbr -> device *-NPN- with package variant TO220 and set

    the VALUE to BUL704.

     

    • 1N914BTR (diode) was not able to find it...

     

    Use diode.lbr -> device DIODE- with package variant DO35-10 and set the

    VALUE to 1N914BTR.

     

     

    And the list is going and going like that on every conponent.

    My frustration level in rising, I spent more time looking ofr the components that I will spend on

    > creating the board (step that I have note reached yet...)

     

    Plase read

    HELP USE (enter)

    HELP ADD (enter)

     

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thank you both for your answers.

    My mail adress is abessy@free.fr ;-)


    I was hoping to spend more time to design the PCB and less on the components selection but I understand that all of them can not exists. It is just hard from the point of view that I am not doing PCB often (in fact it is the first) nor I am working in the electronic field so I am not fluent with the components equivalence (yet).

     

    But I will get at it then...

     

    Thank you again for your answers.

    Regards

    Alexandre Bessy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    badbad2142 wrote:

    Thank you both for your answers.

    My mail adress is abessy@free.fr (mailto:abessy@free.fr) image

     

    I was hoping to spend more time to design the PCB and less on the components selection but I understand that all of them can not exists. It is just hard from the point of view that I am not doing PCB often (in fact it is the first) nor I am working in the electronic field so I am not fluent with the components equivalence (yet).

     

     

    Just a comment from a guy who does electronics design for >25 years:

    Packaging, component selection and the creation of library parts is

    boring but it is often 50% of the job. Especially on cost critical

    designs. So it is very important to learn the library editor of a new

    CAD system very soon. Eagle isn't particularly easy to learn in that

    respect but with persistence you'll get there.

     

    Afterwards, when you haven't used the program for a while it is normal

    to forget things.

     

    By the way, the Digikey search engine is hands down the best there is,

    there ever was. If you learn how to use that (easy) it becomes a

    wonderful tool to find electronic parts. And now they also let you sort

    by price.

     

     

    But I will get at it then...

     

     

    En peu du vin rouge, du fromage et la bonne musique ... and it will all

    come together nicely image

     

    --

    Cordialement, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I was wanting to thank you all for your help. here is the first board I "designed" with your help:

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/Eagle_Board1.jpg

     

    AB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    oh... Thank you Gary for the explanation... I will see if what I have modified in GIMP is acceptable then...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 3/22/2011 7:57 AM, badbad2142 wrote:

    Next question:

    When I am doing a polygone it does not go around the legs of my components but let behind some incovered spots (I understand that a picture would be clearer: http://s203.photobucket.com/albums/aa14/badbad214/Eagle/ ) what is the parameter that I shall change?

     

    It will be hard to solder it without those "thermals" especially if the

    plane is any significant size. It will just act like an infinite heat sink.

     

    This is more an issue for mass produced boards, but it is possible to

    produce a board which is not hand solderable as well, I've worked on

    some that simply have too much heatsinking to the ground plane to

    desolder a component. That's when you get out the hot air tool or put it

    in the oven and hope it survives!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Noep but the funny part is when I am connected it is displayed my real neame when I am not only my pseudo...

     

    Thank you for the hint on thermal.

     

    Hum I would not say that the doc is the most user friendly, an example would have been helpfull in it. What is the syntax for the thermal: Poly Thermal On?

     

    AB

     

    Message was edited by: alexandre bessy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    badbad is your real name???

    Help Polygon is your friend, see the paragraph "Thermals"& the others to

    make your polygon best fit

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Next question:

    When I am doing a polygone it does not go around the legs of my components but let behind some incovered spots (I understand that a picture would be clearer:[IMG]http://i203.photobucket.com/albums/aa14/badbad214/Eagle/Polygon.jpg[/IMG] ) what is the parameter that I shall change?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Works perfectly for me thank you Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 3/21/2011 2:20 PM, badbad2142 wrote:

    I also bake my own but never been able to create a real baguette... here in AR we have the Boulevard Bread which is the closest from the real thing and for the cheese the place is called "the French market" image the taste are Ok but concerning the prices it is another story.

     

    In my Board when I have launched a "Autorouter SetUp" and do not like the result how do I come back to the previous state? (undo doesn't do anything).

     

    Use the ripup command ( type HELP RIPUP), it can also be restricted to

    certain nets, or all nets, or all nets except certain nets.

     

    I recommend you do your critical routes manually first, save it, and

    then autoroute the rest, especially if you have lots of manual routes,

    then it is easy to start over.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I also bake my own but never been able to create a real baguette... here in AR we have the Boulevard Bread which is the closest from the real thing and for the cheese the place is called "the French market" :-) the taste are Ok but concerning the prices it is another story.

     

    In my Board when I have launched a "Autorouter SetUp" and do not like the result how do I come back to the previous state? (undo doesn't do anything).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Gary Gofstein wrote:

    On 3/21/2011 11:20 AM, Joerg wrote:

    >> badbad2142 wrote:

    >>

    >>

    >>

    >>>

    >>> Joerg: I am sad (but also veyr happy) to say that I am currently

    >>> living in the US and undertsand perfectly what you mean concerning

    >>> the cheese!!! Trust me...

    >>>

    >>> image

    >>>

    >>

    >> Costco often carries Boursin, the three-packs with different flavors.

    >> Occasionally they have a Camembert that's actually fairly good if left

    >> outside the fridge for an hour or so. But not very often image

    >>

    >> World Market and Trader Joe's are also good places to hunt for tasty

    >> European cheeses, if you have those store in your area. Bread is another

    >> story and we sometimes bake our own, in the barbecue.

    >>

    always bake my own.

     

     

    Very good. We also bake our pizza in the barbecue, over charcoal. Most

    of the time coals from real firewood. Even when it hails.

     

     

    @OP: lay out your board in mm if you wish ( I often do ),

    but keep schematics at 0.100".

     

     

    Yes, except for library symbols. In order for the more complicated ones

    to look good it is important to switch the grid down to 0.025" or so.

    But make sure outlines and pins are on the 0.100" grid.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    "gmail" domain blocked because of excessive spam.

    Use another domain or send PM.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Gary Gofstein wrote:

    On 3/21/2011 11:20 AM, Joerg wrote:

    >> badbad2142 wrote:

    >>

    >>

    >>

    >>>

    >>> Joerg: I am sad (but also veyr happy) to say that I am currently

    >>> living in the US and undertsand perfectly what you mean concerning

    >>> the cheese!!! Trust me...

    >>>

    >>> image

    >>>

    >>

    >> Costco often carries Boursin, the three-packs with different flavors.

    >> Occasionally they have a Camembert that's actually fairly good if left

    >> outside the fridge for an hour or so. But not very often image

    >>

    >> World Market and Trader Joe's are also good places to hunt for tasty

    >> European cheeses, if you have those store in your area. Bread is another

    >> story and we sometimes bake our own, in the barbecue.

    >>

    always bake my own.

     

     

    Very good. We also bake our pizza in the barbecue, over charcoal. Most

    of the time coals from real firewood. Even when it hails.

     

     

    @OP: lay out your board in mm if you wish ( I often do ),

    but keep schematics at 0.100".

     

     

    Yes, except for library symbols. In order for the more complicated ones

    to look good it is important to switch the grid down to 0.025" or so.

    But make sure outlines and pins are on the 0.100" grid.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    "gmail" domain blocked because of excessive spam.

    Use another domain or send PM.