EAGLE User Support (English) Component replacement
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 1114 views
  • Users 0 members are here
Related

Component replacement

Former Member
Former Member over 14 years ago

Hi there...

 

How can I replace all 0805 size resistors with 0603 resistors.  I have tried

CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.  The

only way it works is if I enter the component name: CHANGE PACKAGE R1 R0603

which means I still have to do individual components...

 

Thanks

Lance

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    On 04/06/2011 08:18 AM, Lance Johnstone wrote:

    Hi there...

     

    How can I replace all 0805 size resistors with 0603 resistors.  I have tried

    CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.  The

    only way it works is if I enter the component name: CHANGE PACKAGE R1 R0603

    which means I still have to do individual components...

     

    This sounds like a job for a ULP.

     

    Spin through all the components on a schematic, then for each component

    check for a package equal to "R0805".  If so, print "change packge Rx

    R0603" to an output file ending with ".scr", then run the script.

     

    Try saving the following ULP in your project directory and running it.

    It will produce a script "test.scr" that you can run from your

    schematic.  This will provide a good example on the ULP language.  It

    can come in very handy for batch oriented tasks such as this and is well

    worthwhile learning.

     

    Enjoy,

        - Chuck

     

    // Make sure we're in a schematic

    if (schematic) schematic(S) {

     

        // Output to a file in the project directory

        output("test.scr", "wt") {

     

            // Spin through the parts on a schematic

            S.parts(P) {

                // For each part...

     

                // ... that has a package

                if (P.device.package) {

     

                    // ... and the name of the package is "R0805"

                    if (strstr(P.device.package.name, "R0805") >= 0) {

     

                        // print a change package command for the part's name

                        printf("change package %s R0603;\n", P.name);

                    }

                }

            }

        }

    }

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago

    On 04/06/2011 08:18 AM, Lance Johnstone wrote:

    Hi there...

     

    How can I replace all 0805 size resistors with 0603 resistors.  I have tried

    CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.  The

    only way it works is if I enter the component name: CHANGE PACKAGE R1 R0603

    which means I still have to do individual components...

     

    This sounds like a job for a ULP.

     

    Spin through all the components on a schematic, then for each component

    check for a package equal to "R0805".  If so, print "change packge Rx

    R0603" to an output file ending with ".scr", then run the script.

     

    Try saving the following ULP in your project directory and running it.

    It will produce a script "test.scr" that you can run from your

    schematic.  This will provide a good example on the ULP language.  It

    can come in very handy for batch oriented tasks such as this and is well

    worthwhile learning.

     

    Enjoy,

        - Chuck

     

    // Make sure we're in a schematic

    if (schematic) schematic(S) {

     

        // Output to a file in the project directory

        output("test.scr", "wt") {

     

            // Spin through the parts on a schematic

            S.parts(P) {

                // For each part...

     

                // ... that has a package

                if (P.device.package) {

     

                    // ... and the name of the package is "R0805"

                    if (strstr(P.device.package.name, "R0805") >= 0) {

     

                        // print a change package command for the part's name

                        printf("change package %s R0603;\n", P.name);

                    }

                }

            }

        }

    }

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Chuck Huber schrieb:

     

    On 04/06/2011 08:18 AM, Lance Johnstone wrote:

    >> How can I replace all 0805 size resistors with 0603 resistors.  I have tried

    >> CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.  The

    >> only way it works is if I enter the component name: CHANGE PACKAGE R1 R0603

    >> which means I still have to do individual components...

     

    This sounds like a job for a ULP.

     

    It should also be possible by command line, i.e.

    change package 'r0603'  ...

    (At least I've done it that way before.)

     

    It should also be possible to apply that command to a group. (Only those

    devices that have the desired package variant will be changed.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Am 06.04.2011 17:30, schrieb Tilmann Reh:

    Chuck Huber schrieb:

     

    >> On 04/06/2011 08:18 AM, Lance Johnstone wrote:

    >>> How can I replace all 0805 size resistors with 0603 resistors.  I have tried

    >>> CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.  The

    >>> only way it works is if I enter the component name: CHANGE PACKAGE R1 R0603

    >>> which means I still have to do individual components...

    >>

    >> This sounds like a job for a ULP.

     

    It should also be possible by command line, i.e.

    change package 'r0603'<klick>  <klick>  <klick>  ...

     

    Far to much to work ..

     

    select elements in BRD with GROUP, type in

     

    CHANGE PACKAGE R-EU_R0603

    btw.

    CHANGE PACKAGE R-US_R0603

                    ^^^^^|

                   

    Name of deviceset   ^^^^^

                         package variant

     

     

    The shortness version:

     

    ch pac R-US_R0603

     

    and now click with rigth mouse button at the group. image

     

    Only elements defined this package in deviceset can change.

     

    TIP:

     

    SET Option.ToggleCtrlForGroupSelectionAndContextMenu 1;

     

    HELP SET (enter)

     

     

    --

     

    Mit freundlichen Grüßen / Best regards

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Aha!!! That's it...  I had done it before, but couldn't remember how...

     

    Thanks for input all of you....

     

     

    "A. Zaffran" <alf@cadsoft.de> wrote in message

    news:injle3$887$2@cheetah.cadsoft.de...

    Am 06.04.2011 17:30, schrieb Tilmann Reh:

    >> Chuck Huber schrieb:

    >>

    >>> On 04/06/2011 08:18 AM, Lance Johnstone wrote:

    >>>> How can I replace all 0805 size resistors with 0603 resistors.  I have

    >>>> tried

    >>>> CHANGE PACKAGE R0805 R0603 and all combinations: 'R0805' 'R0603' etc.

    >>>> The

    >>>> only way it works is if I enter the component name: CHANGE PACKAGE R1

    >>>> R0603

    >>>> which means I still have to do individual components...

    >>>

    >>> This sounds like a job for a ULP.

    >>

    >> It should also be possible by command line, i.e.

    >> change package 'r0603'  ...

     

    Far to much to work ..

     

    select elements in BRD with GROUP, type in

     

    CHANGE PACKAGE R-EU_R0603

    btw.

    CHANGE PACKAGE R-US_R0603

                   ^^^^^|

                   |    |

    Name of deviceset   ^^^^^

                        package variant

     

    >

    The shortness version:

     

    ch pac R-US_R0603

     

    and now click with rigth mouse button at the group. image

     

    Only elements defined this package in deviceset can change.

     

    TIP:

     

    SET Option.ToggleCtrlForGroupSelectionAndContextMenu 1;

     

    HELP SET (enter)

     

    >

    --

     

    Mit freundlichen Grüßen / Best regards

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________