Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Addition of standardized font (ISO-3098)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 1389 views
  • Users 0 members are here
  • anchor
  • eagle
  • iso-3098
  • font
  • standard
Related

Addition of standardized font (ISO-3098)

e14 Contributor
e14 Contributor over 15 years ago

Hi
I have worked some time at a power plant     designing and drawing circuit diagrams for control systems. In this     and presumably many other business it is very important to stick to     standards. My bible during this time was IEC-61082, a     standard that regulates basically every aspect of how to produce and     handle electro-technical documentation.

I like EAGLE a great deal because it is possible to create circuit     diagrams that fulfill at least the important parts of this standard     rather easily. One requirement that schematics made in Eagle always     fails is that all the characters in the diagram must come from the     font defined by the subsidiary standard ISO-3098.

This is a very legible font which can survive an almost infinite     number of runs through a Xerox-machine, a feature that is very     important for documentation that need to be archived. I have spent a     good deal of time first trying to find a free interpretation of     ISO-3098 (font-file) on the Internet and then trying to replace all     text in my schematics with it. With very limited success on the     latter part I might add.

The good thing however is that I found an open-source project,     osifont ( http://code.google.com/p/osifont/ ), that just fills my     needs for a free technical font.

My suggestion is that Cadsoft adds this font to the schematic       editor of Eagle. Legibility of schematics will increase and the       output can be made to comply with IEC-61082. Additionally a more       complete set of anchor points (9, 12, or 15) should be available       to every text-field, as have been suggested many times before. Any       CAD-tool should have the possibility to center text.


Best Regards

Anton Andersson
M.Sc EE

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Maybe we could just have another font selection - a "custom font" besides already existing vector / proportional / fixed. Then anybody could add his favorite font.