EAGLE User Support (English) Difficulty with "power" and "supply"
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
  • Replies 5 replies
  • Subscribers 178 subscribers
  • Views 1528 views
  • Users 0 members are here
Related

Difficulty with "power" and "supply"

Former Member
Former Member over 14 years ago

Hey guys, just just hit the floor with this stuff, so bear with me... I

just created my first device, and it seems to work ok.  The only concept

that's still giving me fits is the PWR and SUP pins. I'm not sure what the

difference is and/or where one is used instead of the other. Also, the use

of +V, Vcc, Vdd, Vss, and GND is giving me a bit of grief.  For example:  I

usually specify +V as the incoming power to the circuit.  Then into the

voltage regulator.  Out of the regulator, I'm faced with the task of

delivering the regulated voltage to my various devices.  Some devices want

Vcc and GND.  Some devices want Vdd and Vss, or some other combination.

Sometimes I power things with the UNregulated buss.  I thought that I could

just add the proper feeds to the downstream side of the regulator or where

ever I want to tap the power, but the ERC just goes nuts, saying that such

and such is overwritten by more than one signal, etc.  Same with the

grounds and/or 0V.  What am I doing wrong?  I've read the parts of the

manual that deal with these concepts over and over again, but I'm just not

getting it.

 

Thanks, Richard

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 14 years ago

    Am 26.04.2011 11:13, schrieb Richard Bennett:

    Hey guys, just just hit the floor with this stuff, so bear with me... I

    just created my first device, and it seems to work ok.  The only concept

    that's still giving me fits is the PWR and SUP pins. I'm not sure what the

    difference is and/or where one is used instead of the other. Also, the use

    of +V, Vcc, Vdd, Vss, and GND is giving me a bit of grief.  For example:  I

    usually specify +V as the incoming power to the circuit.  Then into the

    voltage regulator.  Out of the regulator, I'm faced with the task of

    delivering the regulated voltage to my various devices.  Some devices want

    Vcc and GND.  Some devices want Vdd and Vss, or some other combination.

    Sometimes I power things with the UNregulated buss.  I thought that I could

    just add the proper feeds to the downstream side of the regulator or where

    ever I want to tap the power, but the ERC just goes nuts, saying that such

    and such is overwritten by more than one signal, etc.  Same with the

    grounds and/or 0V.  What am I doing wrong?  I've read the parts of the

    manual that deal with these concepts over and over again, but I'm just not

    getting it.

     

    Thanks, Richard

     

    Hi Richard, don't go down to the electron flow of electricity image

    Help Pin. Here you find about the DIRECTION of pins.

    For power there is a general eagle direction: A battery has a SUPply

    (call it output) of plus and minus, while an IC has PWR (Power)for its

    supply (call that an input). The polarity has nothing to do with it.

    So a three terminal voltage regulator has just an input and an output.

    You can name the output-net anyway you want, or just "clip" a suitable

    supply symbol to it. If you have a schematic then activate layer 93

    (pin) and you can see the pin direction of eagle devices.

    Hope I could help.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    rubyfocus wrote on Tue, 26 April 2011 05:13

    The only concept that's still giving me fits is the PWR and SUP pins.

     

    Yes, the documentation is confusing at best.  The fact that "power pin" and

    "supply pin" are pretty much interchangable in the world outside Eagle

    doesn't help.  Eagle is a nice program, but it's choice of names is

    downright broken in various places.

     

    Basically supply should be used for things like ground symbols.  Connecting

    a supply pin to a net in the schematic effectively overrides the net name

    from the supply pin's name in the library.

     

    Use power for pins of a IC that need to be connected to power or ground.

    Unfortunately the ERC check will complain if a power pin is connected to a

    net that has a different name than itself.  This is a well known Eagle

    stupidity which hopefully will be fixed some day.  For example, you might

    quite reasonably connect a microcontroller Vss pin to a net named GND, or a

    Vdd pin to "5V", but Eagle will complain about the discrepancy.  This is

    just one of the things you have to get used to.

     

    Even worse is that Eagle will implicitly make connections based on the

    names.  I don't remember the exact rules, but I think supply pins are

    automatically connected to nets of their names even if you don't connect

    them.  This is just asking for trouble, but Cadsoft has so far refused to

    fix it.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 04/26/2011 03:06 PM, Olin Lathrop wrote:

    rubyfocus wrote on Tue, 26 April 2011 05:13

    >> The only concept that's still giving me fits is the PWR and SUP pins.

     

    Yes, the documentation is confusing at best.  The fact that "power pin" and

    "supply pin" are pretty much interchangable in the world outside Eagle

    doesn't help.  Eagle is a nice program, but it's choice of names is

    downright broken in various places.

     

    Basically supply should be used for things like ground symbols.  Connecting

    a supply pin to a net in the schematic effectively overrides the net name

    from the supply pin's name in the library.

     

    Use power for pins of a IC that need to be connected to power or ground.

    Unfortunately the ERC check will complain if a power pin is connected to a

    net that has a different name than itself.  This is a well known Eagle

    stupidity which hopefully will be fixed some day.  For example, you might

    quite reasonably connect a microcontroller Vss pin to a net named GND, or a

    Vdd pin to "5V", but Eagle will complain about the discrepancy.  This is

    just one of the things you have to get used to.

     

    Even worse is that Eagle will implicitly make connections based on the

    names.  I don't remember the exact rules, but I think supply pins are

    automatically connected to nets of their names even if you don't connect

    them.  This is just asking for trouble, but Cadsoft has so far refused to

    fix it.

     

    I vastly prefer to call out power pins explicitly on symbols, and to

    make them passive.  This side steps the whole "Eagle knows it's smarter

    than me" routine, it gives me the flexibility I need to put parts on

    different power rails (e.g. when I'm using a 'logic' part in an analog

    circuit, or when I have both 5V and 3V supplies), and it puts power pins

    out in front of anyone reading my schematics, so they know what's

    going on, too.

     

    --

    Tim Wescott

    Wescott Design Services

    Voice: 503-631-7815

    Cell:  503-349-8432

    http://www.wescottdesign.com

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    On 5/2/2011 10:43 AM, Tim Wescott wrote:

    On 04/26/2011 03:06 PM, Olin Lathrop wrote:

    >> rubyfocus wrote on Tue, 26 April 2011 05:13

    >>> The only concept that's still giving me fits is the PWR and SUP pins.

    >>

    >> Yes, the documentation is confusing at best. The fact that "power pin"

    >> and

    >> "supply pin" are pretty much interchangable in the world outside Eagle

    >> doesn't help. Eagle is a nice program, but it's choice of names is

    >> downright broken in various places.

    >>

    >> Basically supply should be used for things like ground symbols.

    >> Connecting

    >> a supply pin to a net in the schematic effectively overrides the net name

    >> from the supply pin's name in the library.

    >>

    >> Use power for pins of a IC that need to be connected to power or ground.

    >> Unfortunately the ERC check will complain if a power pin is connected

    >> to a

    >> net that has a different name than itself. This is a well known Eagle

    >> stupidity which hopefully will be fixed some day. For example, you might

    >> quite reasonably connect a microcontroller Vss pin to a net named GND,

    >> or a

    >> Vdd pin to "5V", but Eagle will complain about the discrepancy. This is

    >> just one of the things you have to get used to.

    >>

    >> Even worse is that Eagle will implicitly make connections based on the

    >> names. I don't remember the exact rules, but I think supply pins are

    >> automatically connected to nets of their names even if you don't connect

    >> them. This is just asking for trouble, but Cadsoft has so far refused to

    >> fix it.

     

    I vastly prefer to call out power pins explicitly on symbols, and to

    make them passive. This side steps the whole "Eagle knows it's smarter

    than me" routine, it gives me the flexibility I need to put parts on

    different power rails (e.g. when I'm using a 'logic' part in an analog

    circuit, or when I have both 5V and 3V supplies), and it puts power pins

    out in front of anyone reading my schematics, so they know what's

    going on, too.

     

    same here. standard operating procedure.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 5/2/2011 10:43 AM, Tim Wescott wrote:

    On 04/26/2011 03:06 PM, Olin Lathrop wrote:

    >> rubyfocus wrote on Tue, 26 April 2011 05:13

    >>> The only concept that's still giving me fits is the PWR and SUP pins.

    >>

    >> Yes, the documentation is confusing at best. The fact that "power pin"

    >> and

    >> "supply pin" are pretty much interchangable in the world outside Eagle

    >> doesn't help. Eagle is a nice program, but it's choice of names is

    >> downright broken in various places.

    >>

    >> Basically supply should be used for things like ground symbols.

    >> Connecting

    >> a supply pin to a net in the schematic effectively overrides the net name

    >> from the supply pin's name in the library.

    >>

    >> Use power for pins of a IC that need to be connected to power or ground.

    >> Unfortunately the ERC check will complain if a power pin is connected

    >> to a

    >> net that has a different name than itself. This is a well known Eagle

    >> stupidity which hopefully will be fixed some day. For example, you might

    >> quite reasonably connect a microcontroller Vss pin to a net named GND,

    >> or a

    >> Vdd pin to "5V", but Eagle will complain about the discrepancy. This is

    >> just one of the things you have to get used to.

    >>

    >> Even worse is that Eagle will implicitly make connections based on the

    >> names. I don't remember the exact rules, but I think supply pins are

    >> automatically connected to nets of their names even if you don't connect

    >> them. This is just asking for trouble, but Cadsoft has so far refused to

    >> fix it.

     

    I vastly prefer to call out power pins explicitly on symbols, and to

    make them passive. This side steps the whole "Eagle knows it's smarter

    than me" routine, it gives me the flexibility I need to put parts on

    different power rails (e.g. when I'm using a 'logic' part in an analog

    circuit, or when I have both 5V and 3V supplies), and it puts power pins

    out in front of anyone reading my schematics, so they know what's

    going on, too.

     

    same here. standard operating procedure.