EAGLE User Support (English) "Copy to library" versus "Remove device"
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 371 views
  • Users 0 members are here
Related

"Copy to library" versus "Remove device"

Former Member
Former Member over 14 years ago

1. Supposing that I need only 1 footprint for LEDs only project;

2. Supposing that I have used the function "Copy to library" to copy LED

component from default library to my library;

3. Supposing that I can live with the fact that I had no choise to choose

what footprint to be copied, and all XXX footprints flooded my "project's

library";

4. Now: supposing that I go in my library and delete the "LED" device,...

guess what?!:

All the footprints that flooded my library (and I had never need of any of

them) remained in my library.

I guess I could remove them one by one, writing on paper the name of each of

one, and then writing by hand that names on the "Remove package" text box.

(PS: and hear the annoiyng beep sound for every footprint removal - but this

is an other thread...). Or I could create a new library right from

scratch... it will be faster...

 

Conclusion: We need a better way to handle components and footprints between

libraries! It s***s in may way as it is now.

 

 

 

 

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 14 years ago

    "eSilviu" <silviu.epure@ugal.ro> wrote in message

    news:iqls53$f6b$1@cheetah.cadsoft.de...

    1. Supposing that I need only 1 footprint for LEDs only project;

    2. Supposing that I have used the function "Copy to library" to copy LED

    component from default library to my library;

    3. Supposing that I can live with the fact that I had no choise to choose

    what footprint to be copied, and all XXX footprints flooded my "project's

    library";

    4. Now: supposing that I go in my library and delete the "LED" device,...

    guess what?!:

    All the footprints that flooded my library (and I had never need of any of

    them) remained in my library.

    I guess I could remove them one by one, writing on paper the name of each

    of one, and then writing by hand that names on the "Remove package" text

    box. (PS: and hear the annoiyng beep sound for every footprint removal -

    but this is an other thread...). Or I could create a new library right

    from scratch... it will be faster...

     

    Conclusion: We need a better way to handle components and footprints

    between libraries! It s***s in may way as it is now.

    >>>>>>>>>>>>>>>>>>>>>>>>>

     

    Arrr. Library editing is CLUNKY at best.

    But there is a way you can expedite (cough cough) the eradication of

    undesired library components:

     

    Suppose you have package called RES_0805 that you want rid of. Go into the

    package editor for that footprint.

    Type 'ren'

     

    It's gone. Light speed it's not, but it works.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 5/16/2011 2:32 PM, Brett Holden wrote:

    "eSilviu"<silviu.epure@ugal.ro>  wrote in message

    news:iqls53$f6b$1@cheetah.cadsoft.de...

    >> 1. Supposing that I need only 1 footprint for LEDs only project;

    >> 2. Supposing that I have used the function "Copy to library" to copy LED

    >> component from default library to my library;

    >> 3. Supposing that I can live with the fact that I had no choise to choose

    >> what footprint to be copied, and all XXX footprints flooded my "project's

    >> library";

    >> 4. Now: supposing that I go in my library and delete the "LED" device,...

    >> guess what?!:

    >> All the footprints that flooded my library (and I had never need of any of

    >> them) remained in my library.

    >> I guess I could remove them one by one, writing on paper the name of each

    >> of one, and then writing by hand that names on the "Remove package" text

    >> box. (PS: and hear the annoiyng beep sound for every footprint removal -

    >> but this is an other thread...). Or I could create a new library right

    >> from scratch... it will be faster...

    >>

    >> Conclusion: We need a better way to handle components and footprints

    >> between libraries! It s***s in may way as it is now.

    >>>>>>>>>>>>>>>>>>>>>>>>>>

    >

    Arrr. Library editing is CLUNKY at best.

    But there is a way you can expedite (cough cough) the eradication of

    undesired library components:

     

    Suppose you have package called RES_0805 that you want rid of. Go into the

    package editor for that footprint.

    Type 'ren'<enter>.

    You are asked what the new name is. I like something short. 'X', for

    instance.

    type 'x'<enter>

    type 'rem x'<enter>

     

    It's gone. Light speed it's not, but it works.

     

    >

    nice trick

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago

    eSilviu wrote:

    1. Supposing that I need only 1 footprint for LEDs only project;

    2. Supposing that I have used the function "Copy to library" to copy

    LED component from default library to my library;

    3. Supposing that I can live with the fact that I had no choise to

    choose what footprint to be copied, and all XXX footprints flooded my

    "project's library";

    4. Now: supposing that I go in my library and delete the "LED"

    device,... guess what?!:

    All the footprints that flooded my library (and I had never need of

    any of them) remained in my library.

    I guess I could remove them one by one, writing on paper the name of

    each of one, and then writing by hand that names on the "Remove

    package" text box. (PS: and hear the annoiyng beep sound for every

    footprint removal - but this is an other thread...). Or I could

    create a new library right from scratch... it will be faster...

     

    Conclusion: We need a better way to handle components and footprints

    between libraries! It s***s in may way as it is now.

     

     

    I agree that additional flexibilty is needed when copying devices. It would

    be good if you could select variant/s as you would then not get all the

    packages of the other variants.

     

    As a possible assist for the LED example given, you could run

    del-pack-sym.ulp

    That would get rid of all the unwanted packages once the LED device was

    deleted. The down side is that if you have other packages that are unused

    but you want to keep you will have to remove them from the script list

    first.

    Try it and see if it works for you.

     

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

     

    "Warren Brayshaw" <warrenbrayshaw@paradise.net.nz> wrote in message

    news:iqsikl$3gh$1@cheetah.cadsoft.de...

    Try it and see if it works for you.

     

    Thank you for suggestion.

    It was faster to create a new library, to copy all needed components from

    the old one and to rename-it as the old one.