In the command line, when I type: ADD LM321@LINEAR
The device is added directly in the schematic without opening the add dialog: it's OK!
But sometimes, when I run a script for adding devices in schematic, I need to check the device in the preview.
So, I need the script command opens the ADD dialog box, show the device and remains open until I click the OK button.
Nota: The Search field in the ADD dialog already do that, but unfortunately, it is not accessible by script.