Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) DXF; output cream layers as "lines", not "solids"?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1297 views
  • Users 0 members are here
  • eagle
  • dxf
  • ulp
  • cam
  • stencil
Related

DXF; output cream layers as "lines", not "solids"?

apullin
apullin over 15 years ago

OK, so I am trying to export some DXF's of the cream layers from Eagle. The purpose is to cut some nice solder paste stencils out of 0.003" stainless shim stock, using our nice 2W UV laser we have here in the lab.

 

The issue is that the dxf.ulp for Eagle exports the pads as "solid" type objects, and, for whatever reason, the laser toolpath generation software doesn't read those correctly. It'll draw 3 sides of a rectangular pad, but not the closing line! The software for the laser isn't very good, and I've put in some inquiries with those folks to see if maybe this problem can be solved from their end.

 

But, if the eagle dxf.ulp exported line perimeters of the solids rather than "solids" themselves, then it should work just fine.

But I guess there are a lot of potential solutions to this... if the dxf.ulp changed it's output format, great. We also have AutoCAD (since they nicely make it free for students), but there doesn't seem to be a straightforward way to convert the "solids" into line segments with that software.

 

I'm reading through the dxf.ulp, and slowly learning the Eagle scripting language. It seems like it should be possible to do it from there.

At the same time, I'm also trying to learn the AutoLISP language, since maybe it can be done via a conversion script inside autoCAD.

If anyone else had any good ideas (python libraries?) that could do this, please do let me know.

 

WMF does work, but doesn't seem to retain scale information. The only way I've gotten it to work so far was by importing both the WMF and the DXF, and using the dimensions of the DXF to scale the WMF imported data.

 

If someone out there just writes the script for me, I'll cut some stencils for you image  (although our laser only does 4" x 4").

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 7/18/11 12:19 AM, Andrew Pullin wrote:

    OK, so I am trying to export some DXF's of the cream layers from Eagle. The purpose is to cut some nice solder paste stencils out of 0.003" stainless shim stock, using our nice 2W UV laser we have here in the lab.

     

    The issue is that the dxf.ulp for Eagle exports the pads as "solid" type objects, and, for whatever reason, the laser toolpath generation software doesn't read those correctly. It'll draw 3 sides of a rectangular pad, but not the closing line! The software for the laser isn't very good, and I've put in some inquiries with those folks to see if maybe this problem can be solved from their end.

     

    But, if the eagle dxf.ulp exported line perimeters of the solids rather than "solids" themselves, then it should work just fine.

    But I guess there are a lot of potential solutions to this... if the dxf.ulp changed it's output format, great. We also have AutoCAD (since they nicely make it free for students), but there doesn't seem to be a straightforward way to convert the "solids" into line segments with that software.

     

    I'm reading through the dxf.ulp, and slowly learning the Eagle scripting language. It seems like it should be possible to do it from there.

    At the same time, I'm also trying to learn the AutoLISP language, since maybe it can be done via a conversion script inside autoCAD.

    If anyone else had any good ideas (python libraries?) that could do this, please do let me know.

     

    WMF does work, but doesn't seem to retain scale information. The only way I've gotten it to work so far was by importing both the WMF and the DXF, and using the dimensions of the DXF to scale the WMF imported data.

     

    If someone out there just writes the script for me, I'll cut some stencils for you image  (although our laser only does 4" x 4").

     

     

    I've had luck printing the tCream layer as an EPS file, importing that

    into Inkscape, changing the fill style of everything to "none" and that

    leaves only outlines.

     

    I save that to PDF since our laser engraver reads those directly. I'm

    not sure if Inkscape can export to DXF.

     

    Andrew.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • apullin
    apullin over 15 years ago in reply to e14 Contributor

    Do you *print* the layer as an EPS, or run it through CAM? Nonetheless ... I'm not sure if I will want to go that route, since it's still pretty circuitous, whereas geometry should "just work"....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • apullin
    apullin over 15 years ago in reply to e14 Contributor

    Do you *print* the layer as an EPS, or run it through CAM? Nonetheless ... I'm not sure if I will want to go that route, since it's still pretty circuitous, whereas geometry should "just work"....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to apullin

    On 7/18/11 5:06 AM, Andrew Pullin wrote:

    Do you print the layer as an EPS, or run it through CAM? Nonetheless ... I'm not sure if I will want to go that route, since it's still pretty circuitous, whereas geometry should "just work"....

     

     

    I run it through CAM.

     

    Andrew.