Hi, I am adding a package to a library, and I need to define a non-plated through hole, OD 1.75mm, for a PCB peg on a Molex connector, see page 2 at http://www.molex.com/pdm_docs/sd/908140808_sd.pdf
I clicked the Hole icon and added a hole. It's now displayed as two concentric circles crossed with a single line, the inner circle has OD 1.75 and the outer circle has OD ~2.0. Why does Eagle display two circles? How can I specify that it's a non-plated hole? Is there any way to specify tolerances for drilling?
Thank you.