Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) CAM Process Create Directories
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 189 subscribers
  • Views 2278 views
  • Users 0 members are here
Related

CAM Process Create Directories

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

I would like to suggest that there be a way for the CAM processor to

automatically create any sub-directories it needs based on the file

specified for a given layer.  For instance, I have the following file

specified for my top layer:

 

%P/gerbers/01-top.grb

 

This structure helps keep the design files separate from the manufacturing

file output.

 

But I have to manually create the gerbers folder which is a bit of a pain.

There is more to this folder structure so it's not just one folder, but

actually a whole tree of folders for various outputs and formats.

 

It would be nice if I could set a switch in the CAM processor to simply

create any sub-directories that it needs that don't exist.

 

James.

 

--

James Morrison  ~~~  Stratford Digital

 

Specializing in CadSoft EAGLE

  • Online Sales to North America

  • Electronic Design Services

  • EAGLE Enterprise Toolkit

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 7/22/2011 7:45 AM, James Morrison wrote:

    Hello,

     

    I would like to suggest that there be a way for the CAM processor to

    automatically create any sub-directories it needs based on the file

    specified for a given layer.  For instance, I have the following file

    specified for my top layer:

     

    %P/gerbers/01-top.grb

     

    This structure helps keep the design files separate from the manufacturing

    file output.

     

    But I have to manually create the gerbers folder which is a bit of a pain.

    There is more to this folder structure so it's not just one folder, but

    actually a whole tree of folders for various outputs and formats.

     

    It would be nice if I could set a switch in the CAM processor to simply

    create any sub-directories that it needs that don't exist.

     

    James.

     

    or even not a switch... just do it.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Gary Gofstein wrote on Fri, 22 July 2011 17:16

    or even not a switch... just do it.

     

    No!  Don't "just do" something that is incompatible with the current

    behavior.

     

    If Eagle had always created subdirectories then I'd probably have my system

    set up to work with that now.  But it doesn't, so I've created my workflow

    around what Eagle does now.  DON'T CHANGE THE DEFAULT.

     

    I use a separate directory for every version of every board, and just put

    all the files in there as one flat pile.  I just checked, and a fairly full

    directory has around 40 files.  That's easily managable without

    subdirectories.  I do have scripts that know the various file name suffixes

    and build the zip files for the board house and for assembly.  These take

    care of the details of grabbing appropriate files from the pile so I don't

    have to.  When I want a file, I know its name and use it directly, so the

    fact that there are 39 other files in the directory is irrelevant.

     

    So for me there is no problem to solve as I've already adapted to how Eagle

    does things.  Add new features if you want, but make sure the default is to

    do the same thing as before.  It would really piss me off if the next

    verion of Eagle did something different out of the box, and I had to waste

    time digging around figuring out how to get it back as it was.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 7/23/2011 6:59 AM, Olin Lathrop wrote:

    Gary Gofstein wrote on Fri, 22 July 2011 17:16

    >> or even not a switch... just do it.

     

    No!  Don't "just do" something that is incompatible with the current

    behavior.

     

    If Eagle had always created subdirectories then I'd probably have my system

    set up to work with that now.  But it doesn't, so I've created my workflow

    around what Eagle does now.  DON'T CHANGE THE DEFAULT.

     

    I use a separate directory for every version of every board, and just put

    all the files in there as one flat pile.  I just checked, and a fairly full

    directory has around 40 files.  That's easily managable without

    subdirectories.  I do have scripts that know the various file name suffixes

    and build the zip files for the board house and for assembly.  These take

    care of the details of grabbing appropriate files from the pile so I don't

    have to.  When I want a file, I know its name and use it directly, so the

    fact that there are 39 other files in the directory is irrelevant.

     

    So for me there is no problem to solve as I've already adapted to how Eagle

    does things.  Add new features if you want, but make sure the default is to

    do the same thing as before.  It would really piss me off if the next

    verion of Eagle did something different out of the box, and I had to waste

    time digging around figuring out how to get it back as it was.

     

    to clarify, i'm not saying that eagle should create subdirectories by

    default. just that if i put a path  in the cam processor with a

    subdirectory that doesn't already exist, eagle should create the

    directory for me like any other program. on v4, it does not, but perhaps

    this was already fixed in v5.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    HI Warren,

     

    Can you show an example!

     

     

    Thanks

     

    Dave M

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    davem wrote:

     

    >.... I cannot currently see how a ULP calls the cam processor,........

     

    You can use the system() function to run the command line version of Eagle

    or eaglecon.exe. With these you can specify that the CAM processor runs.

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    davem wrote:

     

    >.... I cannot currently see how a ULP calls the cam processor,........

     

    You can use the system() function to run the command line version of Eagle

    or eaglecon.exe. With these you can specify that the CAM processor runs.

     

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    HI Warren,

     

    Can you show an example!

     

     

    Thanks

     

    Dave M

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.