Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Whats happening with EagleCad & Cadsoft?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 46 replies
  • Subscribers 191 subscribers
  • Views 5039 views
  • Users 0 members are here
Related

Whats happening with EagleCad & Cadsoft?

e14 Contributor
e14 Contributor over 15 years ago

HI,

 

There have been plenty of user suggestions (including myself ) over the

years and many relating to the same old issues.

 

As a PAYING User, I have essentially invested my money ( but a lot of my

time) into using & Learning EagleCad.

 

So..

 

I would like to know ( from the horses mouth if possible) what is Cadsoft

Proposing/Planning for the next release(s) of Eagle Cad?

Is there an advantage to anyone ( especially users) if future features are

kept secret?

 

The following is what I can see as major changes in no particular order and

not inclusive..

 

Q1) Are there going to be any major changes to the LIBRARY?

 

Q2) Are we going to have a proper user definable /properly integrated BOM

window ?

 

Q3) Can CUT, COPY & PASTE ( and selection/group) work just like any other

application?

 

Q4) Can we open more than one PROJECT or LIBRARY part at the same time?

Will we be able to copy and paste ( Drag and drop) between these?

 

Q5) Can all the user settings and scr files ( or whatever setting files) be

kept in just ONE FILE , in one place and All accessible in ONE User

Preference (TABBED) window? (we can get rid of the Control panel if we do

this, and it means that updating Eaglecad will be less painful).

 

Q6) Are their any plans for some sort of SChematic/Layout hierarchy or

SUB-Circuits feature.

 

Q7) Any plans for a built in Gerber Viewer ( mac users have almost nothing

to work with here?)

 

Q8) Any plans for built in Circuit Simulation ( even basic stuff)?

 

Q9) Any plans for The Built in text editor to have its own Syntax

Highlighting etc?

 

Q10) Any plans for a built in Gerber Panalizer/Merger Tool?

 

Q11) Are there any plans for more control over pads/holes in the device

editor? i.e Odd/Complex shapes.

 

Q12) Can the design link feature work with other suppliers. ( should be

part of the BOM System anyhow)

 

Q13) Can we place less reliance on ULP's and command line entries as a

source of features/enhancements or usability, this should really be only

for specialised tasks. If you have a look at the ULP's over the years

theres a ton of them for Library Management and BOM'S  Is that telling you

something?

 

Q14) Can we have single keystroke functions for at lease basic items, Move,

Change Layer, etc ( user definable of course).

 

I just want to know whats happening, The Beta Test forum is VERY QUIET, The

last release only really had Farnell Shopping added/improved and a few bug

fix's, I am worried that development has either slowed down or stopped. OR

is their  something big in the pipeline. ( hoping!)

 

I am also worried that most suggestions are "Frowned" upon and this really

puts new users off !

 

So that I , ( and everyone else ) can stop wasting our time ( and your

time) with suggestions, can you please answer or give us something to look

forward to?

 

One reason I am asking all the above is that I am considering spending a

LOT OF TIME learning the scripting language so that I can program my own

features ( I have lots of big ideas) , Why, Because I don't know what is

the future for Eaglecad, And I am concerned that I may get to the stage of

writing very useful ULP's and then Cadsoft will release something in the

near future that replaces my work. Remember that all the time I spend

learning the scripting language TAKES ME AWAY From designing boards and

managing production, which is what brings in the money! and besides I

really pay cadsoft for the programming expertise.

 

At the end of the day I believe Eaglecad has a lot of potential, while I

can get boards designed ( its all there as far as capabilities are

concerned) I just think that there are too many frustrating / cumbersome

ways of doing things when I know there are easier /better ways.

 

The designing of a schematic or Layout or even designing a library part is

quite easy ( once you finally figure out the Eaglecad way) , and yes this

is the main parts of an application like this. The issues are with the way

it all comes together or integrates and is managed and how the user

interacts with it. As I have stated above  the key issues are Mainly

Project management, BOM Management, and especially Libray Management.

 

Thanks for listening .

 

Dave M

 

PS Please don't condemn me for asking.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hallo Dave,

     

    some of the things that you mentioned are already possible in current

    EAGLE versions, even if not immediately from scratch:

     

    Am 23.07.2011 09:54, schrieb davem:

    Q8) Any plans for built in Circuit Simulation ( even basic stuff)?

     

    Circuit simulation can be done with an external simulator and some

    dedicated ULP. We are using LTSpice at the moment (aka SwitcherCAD),

    which works well under Windows and Linux (together with Wine). With a

    little bit of luck, I get to know TODAY whether LTSpice can also be used

    together with a Mac. The self-made ULP 'spice' connects the symbol pins

    from the schematic to the corresponding SPICE models, lets the user

    choose settings and runs LTSpice. Connecting to unknown models can be

    done with adding simulator commands as device attributes.

     

    Drawbacks: No crossprobing possible, because LTSpice and EAGLE are

    separate programs. Models need to be downloaded from the IC manufacturer

    and connected 'manually' (this is a problem of license restrictions

    introduced by many IC manufacturers, which explicitely forbid the

    spreading of their models - whyever).

     

    Q9) Any plans for The Built in text editor to have its own Syntax

    Highlighting etc?

     

    The possibility to use an EXTERNAL editor is quite good: CadSoft can

    never hope to produce a text editor that is as good as some external

    tools. For Windows, the (very old) Crimson Editor and the (current)

    Notepad++ make writing ULPs a breeze. I don't know text editors for

    other OSs, but perhaps the above also work using Wine.

     

    Q14) Can we have single keystroke functions for at lease basic items, Move,

    Change Layer, etc ( user definable of course).

     

    You can already put the 'move' command to, e.g., CTRL+M and define key

    combinations for lots of other commands as well. Unfortunately, such key

    combinations are not predefined by CadSoft (they are mainly using

    function keys). If with 'single keystroke' you mean pressing just ONE

    key (and NOT a key combination), this doesn't work (but for the funtion

    keys) due to the command line (which is TOO useful to be abandoned).

    There were several suggestions concerning changing the behaviour of the

    command line, though.

     

    I am concerned that I may get to the stage of

    writing very useful ULP's and then Cadsoft will release something in the

    near future that replaces my work.

     

    As for the BOM, everybody wants a completely different one, so you

    should (with some efforts) create your own with a ULP. What can NOT be

    done properly ULP-wise are things like hierarchical schematics, changing

    pads in the BOARD, arbitrary pad shapes in libraries, etc. some of which

    will apparently be addressed in the next EAGLE version (thanks for the

    info, Mr. Schmidinger).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    HI,

     

    Thanks for the reply Andreas,

     

    I have worked in PCB Assembly Business for several years ( quite some time

    ago) and I can tell you that MOST Bill OF Materials ARE ESSENTIALLY THE

    SAME, from the single engineer to large corporations like Netcomm, Nortel,

    Cisco , Apple etc, I have managed documentation for all types of

    companies.

     

    The only major difference I see in BOMs between small operators and Large

    Corprations is an approved supplier/ approved manufacturers list.

     

    So bom's generally consists of the following fields..

     

     

    Line

    Company Part Number          (optional )

    Qty

    Designators                  (grouped together)

    Description                  (A full description)

    Revision                     (Optional)

    Manufacturer's Name          (A list of Approved manufacturers)

    Manufactures Part Number     (A list of Approved part no's)

    Vendor ( Supplier )          (A list of Approved vendors)

     

    Cost                         (Costs are needed but these are not usually

    passed on)

     

     

    The desciption will usually have all the info, such as ic number,

    footprint, voltage, material type, current rating. enough to make a good

    decision even without the manufacturers part number.

     

    i.e RESISTOR THICK FILM 500mW 200V SMD 1206 1% 5K6

     

    Large corporations will only allow you to purchase from approved

    manufacturers and vendors, both due to testing/quality approvals and supply

    chain deals. They will usually list more than one option and will give an

    order of preference.

     

    Large corporations will also have their OWN PART NUMBERS which would appear

    on a BOM As well.

     

    At the end of the day, I don't see why there are so many types of BOM

    formats! ,  they are all essentially the same ( the order of fields may be

    different, give or take a few fields.

     

    What is different is the way they are received into a business, from plain

    text to spreadsheets (back in my day), and now probably integrated with

    databases but I doubt it.

     

    What I am trying to say that CADSOFT could come up with a BOM SYSTEM that

    would suit 99 percent of everyones needs. Saying that, and just to keep

    everyone happy, it would still be needed to be able to configure the

    format. We could choose the fields and the order of them in a user

    preference window so its used system wide.

     

    I know we can use attributes??, but this FORCES everyone into making

    different set ups so nothing is shared or compatible. thats why we have so

    many ULPS for BOMS.

     

    There is no reason that we can't have a built in window that displays a BOM

    that is kept in "sync" just like the Schematic & Board windows, it would be

    a third button next to the schematic and layout buttons.

     

    I believe the main issue is that CAD Programs Like Eagle cad or any other,

    rely mostly on Generic parts in the library. i.e RESISTOR 0805 10K, as far

    as both the schematic and board layout windows are concerned.

     

    but that shouldn't be a problem, when you first open the BOM Window you

    will just see, the qty , designators (grouped), the footprint and the value

    ( in this case 10K) , Then the main task of the BOM Window is to ASSIGN

    REAL COMPONENTS (Manufactures part numbers) so we know exactly what to

    use/purchase etc.

     

    When you have worked them out, It sort of gives you a TO DO LIST as far as

    assignment of components. This then completes the BOM. Then at anytime, you

    can view this with just one click and no configuration.( after set up in

    our user preferences). From this window you can print it out ( On Paper or

    PDF ) Or you can export to Spreadsheet or text file.

     

    I would like a link to SQL someway so the library and schematics can access

    business databases in both directions.

     

    There is no reason that you could not have your own part numbers in the

    library. ( a variant of a variant???) eg lets say we have an 0805 resistor,

    this would normally be just one part in the eaglecad library, but you may

    create a list of all the resistor values you have ever used i.e say 50

    different values. So thats why we would need a proper PART NUMBER FIELD as

    part of the LIBRARY BOM System.

     

    You would only need to add these parts as you "ASSIGN the PARTS in the

    BOM)

     

    Currently we only have variants which are basically different footprints,

    So I can't see that there is a solution for individual parts. i.e 10k, 5k

    etc within the library system.

     

    I have been thinking long and hard about this issue and I have many ideas.

     

    If I get some time I can make some graphic examples of what I mean. showing

    the user preferences window, sample bom layout window and most important

    the DATA STRUCTURE of how parts info and library info could be managed.

     

    Thanks

     

    Dave M

     

    PS I hope I made some sense??

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello Dave,

     

    Am 26.07.2011 11:58, schrieb davem:

    I have worked in PCB Assembly Business for several years ( quite some time

    ago) and I can tell you that MOST Bill OF Materials ARE ESSENTIALLY THE

    SAME, from the single engineer to large corporations like Netcomm, Nortel,

    Cisco , Apple etc, I have managed documentation for all types of

    companies

     

    Thanks for your thoughts. As a matter of fact, since several weeks, I'm

    thinking about writing a ULP for a BOM also, which would be integrated

    in our documentation system here (and which therefore needs to output

    'LaTeX' code for our PDF documentation). Whether or not a BOM will be

    implemented by CadSoft, I will surely take your ideas into account when

    programming MY program doing that (most of your points I already wanted

    to implement anyway, but there are additional ones that I missed before).

     

    I believe the main issue is that CAD Programs Like Eagle cad or any other,

    rely mostly on Generic parts in the library. i.e RESISTOR 0805 10K, as far

    as both the schematic and board layout windows are concerned.

     

    The main problem is that in order to automatically create a BOM, one

    cannot just look at a device/package pair, but MUST also look at the

    VALUE and should therefore be able to INTERPRET this:

    0.1u=0,1µ=100n=.1uF or 1200R=1,2k=1K2=1.2k etc. Having to add

    manufacturer codes to ALL parts in ALL projects is cumbersome at best,

    so SOME sort of database for looking up default parts is necessary.

     

    Currently we only have variants which are basically different footprints,

    So I can't see that there is a solution for individual parts. i.e 10k, 5k

    etc within the library system.

     

    Yes. Works only with a database somewhere.

     

    With best regards,

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hello Dave,

     

    Am 26.07.2011 11:58, schrieb davem:

    I have worked in PCB Assembly Business for several years ( quite some time

    ago) and I can tell you that MOST Bill OF Materials ARE ESSENTIALLY THE

    SAME, from the single engineer to large corporations like Netcomm, Nortel,

    Cisco , Apple etc, I have managed documentation for all types of

    companies

     

    Thanks for your thoughts. As a matter of fact, since several weeks, I'm

    thinking about writing a ULP for a BOM also, which would be integrated

    in our documentation system here (and which therefore needs to output

    'LaTeX' code for our PDF documentation). Whether or not a BOM will be

    implemented by CadSoft, I will surely take your ideas into account when

    programming MY program doing that (most of your points I already wanted

    to implement anyway, but there are additional ones that I missed before).

     

    I believe the main issue is that CAD Programs Like Eagle cad or any other,

    rely mostly on Generic parts in the library. i.e RESISTOR 0805 10K, as far

    as both the schematic and board layout windows are concerned.

     

    The main problem is that in order to automatically create a BOM, one

    cannot just look at a device/package pair, but MUST also look at the

    VALUE and should therefore be able to INTERPRET this:

    0.1u=0,1µ=100n=.1uF or 1200R=1,2k=1K2=1.2k etc. Having to add

    manufacturer codes to ALL parts in ALL projects is cumbersome at best,

    so SOME sort of database for looking up default parts is necessary.

     

    Currently we only have variants which are basically different footprints,

    So I can't see that there is a solution for individual parts. i.e 10k, 5k

    etc within the library system.

     

    Yes. Works only with a database somewhere.

     

    With best regards,

    Andreas Weidner